Other Parts Discussed in Thread: AM1808, OMAP-L138
Hi Guys,
I am having an interesting problem with the AM1808 processor and LAN8710 (It is a custom board). For some reason u-boot will not recognize the LAN8710 (I have tried logical address 0 and 7, but still no luck). The linux kernel does recognize the MII interface and ifconfig sees it. However I cannot get DHCP addresses allocated to it, and I cannot set up static addresses and make it work.
So my question is, what should I start checking? The oscillator for the LAN8710 is working, and the power supplies are fine.
Best Regards,
Niclas