This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Running into issue using THRLOAD lib along with logging

Hi,

 

I downloaded the THRLOAD lib which is part of the RF modules.

I tried to take the code from the cpuload test project and integrate into a CCS v4 project I have.

Everything is compiling fine except that it can't find logTrace (this is defined as an extern function in cpuload.c).

The only reference I found for the function is in a .cdb file under C:\Program Files (x86)\rf_modules\ti\rf\test\thrload\cpuload_64_Dsk6416. Based on timestamp, the Dsk6416 directory was built as a result of the CCS build, so the .cdb file is either auto-generated, or was copied from somewhere.

My question is, where is the logTrace function defined, so that I can copy that function into my independent CCS v4 project.

 

Thanks, Peter