I have a new board with a TMS320C6748 whose reset line is asserted. I cannot figure out what is pulling the reset line down. I have disconnected everything except for an FPGA, which I cannot disconnect b/c it runs on an internal layer, and the line is still pulled low. I confirmed that other lines from the same FPGA bank are tristated, but I cannot prove the FPGA is not driving reset.
If I pull it up through a 200 ohm resistor, it rises to 0.5V. If I pull it up through a 100 ohm resistor, it goes to 1.1V. My ammeter placed between 3.3V to reset shows 27mA. Resistance of DSP_RST when board is unpowered is in the low k ohm range.
I am not detecting any shorts to adjacent pads on the DSP or FPGA.
I am going to attempt to get into the FPGA and verify it's not asserting output on the line.
My question for TI is whether there is any failure mode you know of that could cause the DSP's reset input to pull its net down.
Thanks!!
CJ