I burn my project into flash.But the project in emulation mode can run two times as fast as in boot mode .
Why?
could you help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I burn my project into flash.But the project in emulation mode can run two times as fast as in boot mode .
Why?
could you help me?
Can you please give more details ?
What does your program actually do ?
Which Flash device ?
The program is aim to make led lights sprink preriodly.I use DM6437,and the datawidth of the flash is 8bit.The bootmode is fastboot from ROM with AIS.When I emulate the program with emulator ,the led lights sprink normal,but after I burn the program into flash ,and power on, the led lights sprink more slowly.