Dear,
I have used TDA4VM, and tested demo 'Vision Apps' successfully.
But now I get the error messages when I connect the board with UART in SD card boot mode.
I reinstalled Linux system(Ubuntu 18.04) and PSDK LA+RA and got same error message. Could you help?
I attach the error message.
Regards,
Yongcheon.
-------------------------------------------------------------------------------------------
Welcome to minicom 2.7.1
OPTIONS: I18n
Compiled on Aug 13 2017, 15:25:34.
Port /dev/ttyUSB0, 16:52:40
Press CTRL-A Z for help on special keys
U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:25 +0000)
SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.0-v2019.08 (Terrific Llama')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Remoteproc 2 started successfully
** File not found /lib/firmware/j7-mcu-r5f0_0-fw **
Starting ATF on ARM64 core...
NOTICE: BL31: v2.1(release):ti2019.02-rc4
NOTICE: BL31: Built : 03:52:00, Oct 24 2019
I/TC:
I/TC: OP-TEE version: ti2019.02-89-ge5a8779-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Thu O4
I/TC: Initialized
U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000)
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
U-Boot 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000)
SoC: J721E PG 1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E6
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: eth0: ethernet@046000000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
** Unable to read file boot.scr **
81 bytes read in 1 ms (79.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
ethernet@046000000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
phy_startup failed
am65_cpsw_start end error
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
=>