Other Parts Discussed in Thread: OMAP-L137, DA8XX
Hi,
I am trying to make my OMAPl137 board boot from usb. I fallowed the steps written in thisPage. I am using DaVinci-PSP-SDK-03.20.00.08. According to document in linked page, I created 2 partitions, one for uImage, one for file system. Although it finds and loads kernel, it gives up kernel panic error. I think it could'nt find filesystem paritition. I've tried some variations of filesystem parition such as sda1, sda2, sdb1, sdb2. Nothing changed, I still get the same error. I add boot msg record below. Do you haveany idea why I get that kernel panic error.
U-Boot 1.3.3 (Oct 15 2009 - 10:48:45)
I2C: ready
DRAM: 64 MB
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
More than one PHY detected.
Hit any key to stop autoboot: 0
(Re)start USB...
USB: scanning bus for devices... 1 USB Device(s) found
scanning bus for storage devices... 1 Storage Device(s) found
reading uImage
...............................................................................................................................................................................
1821232 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.32-rc6
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1821168 Bytes = 1.7 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux........................................................................................................................ done, booting the kernel.
Linux version 2.6.32-rc6 (linuxdev@linuxdevPC) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 PREEMPT Mon Jan 17 16:24:31 EET 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA830/OMAP-L137 EVM
Memory policy: ECC disabled, Data cache writethrough
DaVinci da830/omap-l137 rev1.1 variant 0x8
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: console=ttyS2,115200n8 noinitrd rw ip=off root=/dev/sda1 rootfstype=ext2 mem=32M
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 28584KB available (3456K code, 261K data, 144K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 128 gpio irqs
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pcf857x: probe of 1-003f failed with error -121
Switching to clocksource timer0_0
musb_hdrc: version 6.0, cppi4.1-dma, (host+peripheral), debug=0
musb_hdrc: USB OTG mode controller at fee00000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 55
io scheduler noop registered
io scheduler anticipatory registered (default)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
Read MAC addr from EEPROM: 00:0e:99:02:fb:5e
m25p80 spi0.0: w25x32 (4096 Kbytes)
Creating 3 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000044000 : "U-Boot Environment"
0x000000044000-0x000000400000 : "Linux"
davinci SPI Controller driver at 0xfec41000 (irq = 20) use_dma=1
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 2
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb2: configuration #1 chosen from 1 choice
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
g_ether gadget: using random self ethernet address
g_ether gadget: using random host ethernet address
usb0: MAC 0e:ff:ab:66:0e:26
usb0: HOST MAC 06:4e:79:09:b9:51
g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
g_ether gadget: g_ether ready
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
watchdog watchdog: heartbeat 60 sec
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: v2.6:USB HID core driver
usb 1-1: new high speed USB device using musb_hdrc and address 2
Advanced Linux Sound Architecture Driver Version 1.0.21.
No device for DAI tlv320aic3x
asoc: tlv320aic3x <-> davinci-i2s mapping ok
mmc0: host doesn't support card's voltages
mmc0: error -22 whilst initialising SDIO card
ALSA device list:
#0: DA830/OMAP-L137 EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused emac
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2000-01-03 20:05:16 UTC (946929916)
Root-NFS: No NFS server available, giving up.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "sda1" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 256 mtdblock0 (driver?)
1f01 16 mtdblock1 (driver?)
1f02 3824 mtdblock2 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Best Regards
Hasan