Other Parts Discussed in Thread: AM4372, AMIC120
Hi every all !!!
I am designin my hardware bsaed in AM4372, I hace 2 question please,
1-) The AM4372 has witdh in the ram data bus (DQ0-DQ31) of 23 bits.
Can I connect only one memory RAM of 16 bits in the low half of the bus (D0-D15) ?
If yes, what I must to do with hight half of the bus (D16-D31)? I must keep open or pulled?
2-) In the refence design: AM437x StarterKit EVM, there are a flash memory MX66L51235FMI. Can I removed it in my custom desing? I my design I have a eMMC NAND flash.
Thanks very much. Best Regards