This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4372: LPDDR2 interface at OPP50

Part Number: AM4372

We have one quires regarding to processor selection

Does VDD MPU OPP OPP50 ARM9 300MHz support the LPDDR2?

If Yes then at what frequency it communicate.

reply us as soon as possible

Thanks you.

  • Paresh Parekh1 said:
    Does VDD MPU OPP OPP50 ARM9 300MHz support the LPDDR2? If Yes then at what frequency it communicate?

    See Table 5-1 in the AM437x Datasheet Rev. E.

    Paresh Parekh1 said:
    Does OPP50 processor used for the L1 Register device?

    I don't understand this question. Please clarify.