This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H12: How to know DSP operating frequency

Part Number: 66AK2H12

Hi Everyone,

We are using k2h EVM with processor sdk linux 06_01_00_08, we want to know at which speed DSP is operating?

Regards,

Snehal

  • Hi, Snehal,

    in U-boot prompt, type "getclk" it would show you the usage of it. 

    Rex

  • Hi Rex,

    Its gives the following,

    -Boot
    => getclk
    getclk - get clock rate

    Usage:
    getclk <clk index>
    The indexes for clocks:
    0 - core_pll_clk
    1 - pass_pll_clk
    2 - tetris_pll_clk
    3 - ddr3a_pll_clk
    4 - ddr3b_pll_clk
    5 - sys_clk0_clk
    6 - sys_clk0_1_clk
    7 - sys_clk0_2_clk
    8 - sys_clk0_3_clk
    9 - sys_clk0_4_clk
    10 - sys_clk0_6_clk
    11 - sys_clk0_8_clk
    12 - sys_clk0_12_clk
    13 - sys_clk0_24_clk
    14 - sys_clk1_clk
    15 - sys_clk1_3_clk
    16 - sys_clk1_4_clk
    17 - sys_clk1_6_clk
    18 - sys_clk1_12_clk
    19 - sys_clk2_clk
    20 - sys_clk3_clk
    21 - uart_pll_clk

    is core_pll_clk is DSP operating frequency?

    its gives following

    => getclk 0
    clock index [0] - frequency 1200000000
    =>

    From the board file in u-boot board_k2hk.c

    What is the significance of alt_core_clk ?

    [u-boot code]

    unsigned int get_external_clk(u32 clk)
    {
    unsigned int clk_freq;

    switch (clk) {
    case sys_clk:
    clk_freq = 122880000;
    break;
    case alt_core_clk:
    clk_freq = 125000000;
    break;

    ...

    Regards,

    Snehal

  • Hi, Snehal,

    Yes, the core_pll_clk is the one. type "getclk 0" you should see the frequency for DSP.. I don't know what alt_core_clk is for on top of my head. I'll let you trace the code to see what that is used for. I will have to trace it myself too.

    Rex