Part Number: TDA4VMXEVM
Hi TI,
I have tested the custom kernel in the host emulation mode and c66x, however, the performance is quite poor on the target even though I have implemented a simple color conversion. At first, the target is to implement and running some more complex functions (i.e functions not available in TI supported libs) which are/will be written in C, using whatever the computational resources available on TDA4 to finish the pipeline and then jump into optimization of those functions. Keeping this background in mind, I have following questions:
1. What are the most powerful units that can implement C based functions and give similar performance as on host?
2. Regarding the ARM, I am bit confused with the reference names used, If my Core.ARM what should be the targets? IPUs, R5Fs, VPAC_MSC1, A72, so on ... which are better to pick at first? Any document which explain these naming conventions will also be helpful.
With best regards,
H.M. Owais