Hello,
in U-Boot after following modification (to boot from eMMC)
-----
mmc dev 0
setenv bootargs console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 vm.overcommit_ratio=5 vm.overcommit_memory=2 root=/dev/mmcblk0p1 ip=dhcp
setenv bootcmd "setenv autoload no;ext4load mmc 0:1 0x82000000 /boot/Image;ext4load mmc 0:1 0x81200000/boot/k3-j721e-common-proc-board.dtb; booti 0x82000000 - 0x81200000"
saveenv
-----
I'm no longer able to boot from micro-SD.
Would you please provide me a procedure to store the right values to boot again from micro-SD.
How to switch back
-----------------------------------------------------------------------------
U-Boot SPL 2019.01-g66126341c8 (Dec 11 2019 - 21:52:37 +0000)
SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.1-v2019.08b (Terrific Llam')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Remoteproc 2 started successfully
** File not found /lib/firmware/j7-mcu-r5f0_0-fw **
Starting ATF on ARM64 core...
NOTICE: BL31: v2.1(release):ti2019.02-rc4
NOTICE: BL31: Built : 21:52:04, Dec 11 2019
I/TC:
I/TC: OP-TEE version: ti2019.02-89-ge5a8779-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Wed Dec 11 21:52:32 UTC 2019 aarch64
I/TC: Initialized
U-Boot SPL 2019.01-g66126341c8 (Dec 11 2019 - 21:52:51 +0000)
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
ti_sci_power_domain_on: get_device(91) failed (-19)
U-Boot 2019.01-g66126341c8 (Dec 11 2019 - 21:52:51 +0000)
SoC: J721E PG 1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM: 4 GiB
Flash: 0 Bytes
MMC: ti_sci_power_domain_on: get_device(91) failed (-19)
sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: eth0: ethernet@046000000
Hit any key to stop autoboot: 0
** Unrecognized filesystem type **
** Unrecognized filesystem type **
Bad Linux ARM64 Image magic!
=>
=> printenv
arch=arm
args_all=setenv optargs earlycon=ns16550a,mmio32,0x02800000 ${mtdparts}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
args_ufs=setenv devtype scsi;setenv bootpart 1:1;run ufs_finduuid;setenv bootargs console = ${console} ${optargs}root=PARTUUID=${uuid} rw rootfstype=${scsirootfstype};setenv devtype scsi;setenv bootpart 1:1
autoload=no
baudrate=115200
board=j721e
board_name=J721EX-PM2-SOM
board_rev=E7
board_serial=0143
board_software_revision=01
boot=mmc
boot_fit=0
boot_rprocs=if test ${dorprocboot} -eq 1 && test ${boot} = mmc; then rproc init;run boot_rprocs_mmc;fi;
boot_rprocs_mmc=env set rproc_id;env set rproc_fw;for i in ${rproc_fw_binaries} ; do if test -z "${rproc_id}" ; then env set rproc_id $i;else env set rproc_fw $i;run rproc_load_and_boot_one;env set rproc_id;env set rproc_fw;fi;done
bootargs=console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 vm.overcommit_ratio=5 vm.overcommit_memory=2 root=/dev/mmcblk0p1 ip=dhcp
bootcmd=setenv autoload no;ext4load mmc 0:1 0x82000000 /boot/Image;ext4load mmc 0:1 0x81200000/boot/k3-j721e-common-proc-board.dtb; booti 0x82000000 - 0x81200000
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootpart=1:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
check_android=setenv mmcdev 0; env delete boot_start; part start mmc ${mmcdev} boot boot_start; if test "$boot_start" = ""; then env set is_android 0; else env set is_android 1; fi; env delete boot_start
check_dofastboot=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; env save; echo Booting into fastboot ...; fastboot 0; fi
console=ttyS2,115200n8
cpu=armv8
dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
dfu_alt_info_mmc=boot part 1 1;rootfs part 1 2;tiboot3.bin fat 1 1;tispl.bin fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1;sysfw.itb fat 1 1
dfu_alt_info_ospi=tiboot3.bin raw 0x0 0x080000;tispl.bin raw 0x080000 0x200000;u-boot.img raw 0x280000 0x400000;u-boot-env raw 0x680000 0x020000;sysfw.itb raw 0x6c0000 0x100000;rootfs raw 0x800000 0x3800000
dfu_alt_info_ram=tispl.bin ram 0x80080000 0x100000;u-boot.img ram 0x81000000 0x100000
dfu_bufsiz=0x20000
dorprocboot=0
emmc_android_boot=echo Trying to boot Android from eMMC ...; run update_to_fit; setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 0; mmc dev $mmcdev; mmc rescan; part start mmc ${mmcdev} boot boot_start; part size mmc ${mmcdev} boot boot_size; mmc read ${fit_loadaddr} ${boot_start} ${boot_size}; run get_overlaystring; run run_fit
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
eth1addr=70:ff:76:1d:98:8a
eth2addr=70:ff:76:1d:98:8b
eth3addr=70:ff:76:1d:98:8c
eth4addr=70:ff:76:1d:98:8d
ethaddr=50:51:a9:fc:83:1e
fdtaddr=0x82000000
fdtcontroladdr=fdec3808
findfdt=if test $board_name = J721EX-PM2-SOM; then setenv fdtfile k3-j721e-common-proc-board.dtb; fi;if test $board_name = J721EX-PM1-SOM; then setenv fdtfile k3-j721e-proc-board-tps65917.dtb; fi;setenv overlay_files ${name_overlays}
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage
fit_loadaddr=0x90000000
get_fdt_mmc=load mmc ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
get_fdt_ufs=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
get_kern_mmc=load mmc ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
get_kern_ufs=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
get_overlay_mmc=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $overlay_files;do;load mmc ${bootpart} ${overlayaddr} ${bootdir}/${overlay} && fdt apply ${overlayaddr};done;
get_overlay_ufs=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load scsi ${bootpart} ${overlayaddr} ${bootdir}/${overlay} && fdt apply ${overlayaddr};done;
get_overlaystring=for overlay in $overlay_files;do;setenv overlaystring ${overlaystring}'#'${overlay};done;
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
init_mmc=run args_all args_mmc
init_ufs=ufs init; scsi scan; run args_ufs
loadaddr=0x80080000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_mmc; run run_fit;
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mainr5f0_0fwname=/lib/firmware/j7-main-r5f0_0-fw
mainr5f0_0loadaddr=88000000
mcur5f0_0fwname=/lib/firmware/j7-mcu-r5f0_0-fw
mcur5f0_0loadaddr=89000000
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test ${boot_fit} -eq 1; then run loadfit; else run mmcloados;fi;fi;fi;
mmcdev=1
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
mtdids=nor0=47040000.spi.0,nor0=47034000.hyperbus
mtdparts=mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs)
name_kern=Image
overlayaddr=0x83000000
partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
partitions_android=uuid_disk=${uuid_gpt_disk};name=bootloader,start=5M,size=8M,uuid=${uuid_gpt_bootloader};name=tiboot3,start=4M,size=1M,uuid=${uuid_gpt_tiboot3};name=boot,start=13M,size=40M,uuid=${uuid_gpt_boot};name=vendor,size=1024M,uuid=${uuid_gpt_vendor};name=system,size=2048M,uuid=${uuid_gpt_system};name=userdata,size=-,uuid=${uuid_gpt_userdata}
rd_spec=-
rproc_fw_binaries=3 /lib/firmware/j7-main-r5f0_1-fw 4 /lib/firmware/j7-main-r5f1_0-fw 6 /lib/firmware/j7-c66_0-fw 7 /lib/firmware/j7-c66_1-fw 8 /lib/firmware/j7-c71_0-fw
rproc_load_and_boot_one=if load mmc ${bootpart} $loadaddr ${rproc_fw}; then if rproc load ${rproc_id} ${loadaddr} ${filesize}; then rproc start ${rproc_id};fi;fi
run_fit=bootm ${fit_loadaddr}#${fdtfile}${overlaystring}
run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
scsirootfstype=ext4 rootwait
serial#=0000000000000143
soc=k3
stderr=serial@2800000
stdin=serial@2800000
stdout=serial@2800000
ufs_finduuid=part uuid scsi ${bootpart} uuid
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
vendor=ti
Environment size: 7059/131067 bytes
=>