This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: eMMC programming from USB RNDIS fails

Part Number: AM3358

Hi,

I have followed the process to flash emmc of beaglebone black board using USB RNDIS by this process https://processors.wiki.ti.com/index.php/Sitara_Linux_Program_the_eMMC_on_Beaglebone_Black. 

I have getting error,  mention below. I want to know whether the issue with image or booting process?

U-Boot SPL 2018.11 (Jan 30 2019 - 18:06:42 -0600)
Trying to boot from USB eth
Loading Environment from FAT... Card did not respond to voltage select!
usb_ether
Error: usb_ether address not set.

using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC d0:39:72:97:89:26
HOST MAC de:ad:be:ef:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
high speed config #2: 2 mA, Ethernet Gadget, using RNDIS
USB RNDIS network up!
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17

Retry time exceeded; starting again
Problem booting with BOOTP
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Regards,

Shubham