Part Number: DRA744
Hi,
I am working on a system with DRA74x CPU.
I want to add a lvds display to the system (1280 x800)
Following are excerpts of the schematics for the LCD connections.
Vout3 parallel output RGB888 is connected to SN65LVDS93AIDGGRQ1 which converts it to a LVDS signal.
how do I add device tree entries for these in the dts files?
kindly, shed some light on this.
Regards,
Vijay Jadhav