This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Android on AM572xGPEVM

Part Number: AM5728

Dear Sirs:

  We are using AM5728GPEVM rev.A

And we try PSDK Android AM57x 06_01_00_08 and PSDK Android AM57x 05_03_00_07. However after build the AFS and related code and flash it into the board, we are not able to fully boot the 5728GPEVM, and it will crash during boot and finally reboot.

  My question is that can the PSDK Android 06_01_00_08 or 05_03_00_07 run on AM5728GPEVM rev.A?

  By the way, the GPEVM H/W is good because it can run the latest AM57x RTOS SDK and latest Linux RT SDK with problem.

  Any comments are welcome.

Regards,

/ckhsu