Hi,
I am working on the power management feature of DM6467.
The DSP Bios version is 5.41.00.06
My query is
1) Does the above DSP bios mentioned above support low power mode. ie does the DSP enter low power mode when idling.
2) Is it possible to know on the ARM side that the DSP is idling and hence it clocks can be turned off?
3) As per the documention to put the C64+ DSP clocks can be turned off via ARM core using the associated mode control registers(LPSC).
Regards
Mohammed Anwar