Hi TI Team,
We are working on TDA4 based our hardware and we have specific questions on CPSW-2G and CPSW-9G Eth Switch. Please provide the response the following queries.
Q1 | What are the default CPSW-9G switch PORT settings when TDA4 software is loaded ? i.e. RGMII, RMII, GMII Please provide the source path of the software where this configuration are located. |
Q2 | In our hardware design - we have connected external SoC to PORT 2 of CPSW-9G via RGMII interface, do we need to change register settings on TDA4 software SDK 06.02.00 to make link up and running with external device ? If the answer is yes, where do we need to do changes in software to PORT 2 work for external device for RGMII interface. |
Q3 | Please help to clarify the following doubts, Working SET UP: Our connection to MCU_RGMII1 PORT <--> External PHY <--> RJ45 connector <--> PC or ethernet device - MCU_RGMII1 PORT on CPSW-2G is connected to MCU R5 core, but we are able to communicate from Linux on A72 core to PC (via RJ45). Doubt: Is there any internal communication between MCU R5 and Linux A72 ? IF it is yes, what is the underneath communication interface ? |