This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPEG4 encoder failure on DM355



Hello Champs,

My customer experiences the problem with MPEG4 encoder on DM355 IPNC - when they add SVH parameter to IMP4VENC_Params structure. For the rest parameters (and with default parameters as well) encoder works but gives artefacts in the video - see attached snapshot. Please advise how to improve quality of the encoder using additional parameters?
When they add SVH parameter encoder fails and is not created. (some more information on the failure is here (logs):

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/int-dm3x/f/101/p/87804/303560.aspx

Best regards,
Ilya