This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Dear TI:
I'm need to computer the performance of a imported model。
as the doc,running the imported model in PC simulation,get the result,
but actually I want to know the performance on TI Jacinto7 EVM,
there are some usecase of TIDL at vision_apps,if I want execute myself models,can I run the imported model like doc (j7 in no-boot mode,use CCS)(file:///D:/tda4/TDA4_NEW/psdk_rtos_auto_j7_06_01_01_docs_only/tidl_j7_01_00_01_00/ti_dl/docs/user_guide_html/md_tidl_user_model_deployment.html)
or need add a usecase of myself at dl_demos like app_tidl。
is the two way‘s performance are same if execute the same model。
tks Nigel
In both methods, performance would be the same (vision_apps based app may slight variation based on other system DDR traffic).
We would recommend using the below method for performance validation