Hi,
We're using the Am3354 with 2 devices on GPMC, an 8-bit asynchronous NAND, and a 16-bit NOR type asynchronous device.
Question 1 - Can the Destination Address mode of CONST be used? I don't see anything in SPRUH73 that says it can't, but just want to be sure. It's not a NOR flash, but uses the NOR mode.
Question 2 - Can both GPMC devices use DMA? I'm NOT well versed in the EDMA controller, but see just the single GPMCEVT, which makes me wonder.
Thanks for your help.