Hello,
We have the trouble for the boundary scan test on AM5728.
We found several mismatches about the results of the test.
Could you confirm why the mismatches occur?
The following pins have the issue.
-J7, J4, J6, H4, H5, K7, J5, K6
These pins are set to GPIO. Although output values are expected to be read, the read value is fixed to Low.
-U25
This pin is set to DDR3 WE#. Although output values are expected to be read, the read value is fixed to Low.
-C27, D27
These pins are set to UART1_RTSN and UART1_DTRN. Although output values are expected to be read, the read value is fixed to Low.
-M3
This pin is set to GPIO. Although, we can read the value from the connected device to this pin, the output value of the pin cannot be read at the connected device.
We use the BSDL file on the web to test.
AM572x BSDL Models (Rev. B) BSDL Model ZIP 17 Nov 2017
Best Regards,
Nomo