Part Number: DRA726
Other Parts Discussed in Thread: TDA2,
I am working on getting our cameras supported in IPU1 and have a question on Virtual DRM
I have been reading "Virtual DRM : An User Guide for Developing Usecases". It seems straightforward but doesn't address my use case.
We have two possible LCD displays, one 7 inch display 800x1280 and one 12 inch display 1920x720
The board is the same except for some jumpers that choose the proper LVDS serial format. No way to know from u-boot or Linux which jumpers are populated.
How would I handle that in the M4 and on Linux if I want only one u-boot and one linux kernel?
I would also be nice if the 7 inch display was seen as 1280x800 so the Linux software wouldn't have to flip the LCD 90 degrees
Michel Catudal
ACTIA Corp