Part Number: AM5746
Hello,
I am using Processor SDK 06.02.00.81.
I have added docker and python-docker-compose to the build.
IMAGE_INSTALL_append = " openssh docker python3-docker-compose openjdk-8"
When running docker-compose in the image, it results in a docker version mismatch error:
root@am57xx-evm:/usr/bin# docker-compose
Traceback (most recent call last):
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 573, in _build_master
ws.require(__requires__)
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 891, in require
needed = self.resolve(parse_requirements(requirements))
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 782, in resolve
raise VersionConflict(dist, req).with_context(dependent_req)
pkg_resources.ContextualVersionConflict: (docker 3.4.0 (/usr/lib/python3.5/site-packages), Requirement.parse('docker<3.0,>=2.5.1'), {'docker-compose'})
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "/usr/bin/docker-compose", line 6, in <module>
from pkg_resources import load_entry_point
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 3098, in <module>
@_call_aside
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 3082, in _call_aside
f(*args, **kwargs)
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 3111, in _initialize_master_working_set
working_set = WorkingSet._build_master()
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 575, in _build_master
return cls._build_from_requirements(__requires__)
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 588, in _build_from_requirements
dists = ws.resolve(reqs, Environment())
File "/usr/lib/python3.5/site-packages/pkg_resources/__init__.py", line 777, in resolve
raise DistributionNotFound(req, requirers)
pkg_resources.DistributionNotFound: The 'docker<3.0,>=2.5.1' distribution was not found and is required by docker-compose
root@am57xx-evm:/usr/bin#
Can you please provide guidance on how to fix. Thank you.