Part Number: TDA4VMXEVM
I have asked a related question before: https://e2e.ti.com/support/processors/f/791/p/896299/3313401
But, This doesn't completely solve my problem.
I have 2 input in ModelB. The scale of input_1 is s_1 and the scale of input_2 is s_2.
I have set as following in my import configuration file:
inQuantFactor = s1 s2
inDataNameList = "input_1, input_2"
But in the trace log I can see the scales of input_1 and input_2 are both s1.
Can I set the scale for the two inputs separately?