Part Number: TDA3XEVM
hi i'm using visiond_sdk_03_05.
i want to see zoom effect.
my uscase is IssCapture->custoalgo->IssM2mIsp->IssM2mSimcop->Display
inputdataformat is raw data and output is YUV_420
there are several method to cropping, use Isp or dss \
i want to update displayed image based on user preference of X,Y start position , cropsize and scalefactor coordinate so i am in a need to pass these dynamic parameters to display link.
i saw a technical reference tda3x, isp can crop and resize
so i change link paramter and see the crop image. but when i use scale facotr, i can't see any display image
use dss or isp what is correct?