Part Number: AM3352
Hello,
We are using am3352 in our design with kernel 4.14.67 from TI SDK. We were using a previous U-Boot version and now we moved to 2019.01 from TI.
Porting is done to our board and it is working fine, but we have a problem with the default start-up.
In the previous version default start-up was showing some traces and login/password on serial console (ttyO4) .
In this new version only "U-Boot 2019.01-1.0.11+ (Apr 07 2020 - 10:02:31 +0200)" is shown and it is not possible to login on serial console.
But, if we stop at u-boot prompt and run "boot" command then serial console is again ready for login into the system.
Could you please help us to find what we need to change to set the serial console as dafault to login into the system?
Best regards and thank you
Angel