hello!
I met such a question, I make omap3530 board only left uart and usb , can I download x-loader,u-boot,kernel,and rootfs? thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello!
I met such a question, I make omap3530 board only left uart and usb , can I download x-loader,u-boot,kernel,and rootfs? thank you!
You can refer below page,
http://processors.wiki.ti.com/index.php/AM35x-OMAP35x-PSP_03.00.00.05_UserGuide#MUSB_Host_Support
Regards,
Ajay
If uboot is corrupted then USB can't be used to download/update x-load/uboot binaries. I think you can use UART kermit command to transfer binaries in this case on OMAp35x.
Ajay
Also you can use JTAG interface (if available) to download and execute x-loader/u-boot to get u-boot prompt and then flash it.
Thanks,
Vaibhav