Hello all,
Our customer has a concern about ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install.bin having the CBE issues below, and we really need TI SDK expert's help.
Really appreciate it.
CVE-2020-11494
An issue was discovered in slc_bump in drivers/net/can/slcan.c in the Linux kernel through 5.6.2. It allows attackers to read uninitialized can_frame data, potentially containing sensitive information from kernel stack memory, if the configuration lacks CONFIG_INIT_STACK_ALL, aka CID-b9258a2cece4.
CVE-2019-19076
** DISPUTED ** A memory leak in the nfp_abm_u32_knode_replace() function in drivers/net/ethernet/netronome/nfp/abm/cls.c in the Linux kernel before 5.3.6 allows attackers to cause a denial of service (memory consumption), aka CID-78beef629fd9. NOTE: This has been argued as not a valid vulnerability. The upstream commit 78beef629fd9 was reverted.
CVE-2019-19080
Four memory leaks in the nfp_flower_spawn_phy_reprs() function in drivers/net/ethernet/netronome/nfp/flower/main.c in the Linux kernel before 5.3.4 allow attackers to cause a denial of service (memory consumption), aka CID-8572cea1461a.
CVE-2019-19081
A memory leak in the nfp_flower_spawn_vnic_reprs() function in drivers/net/ethernet/netronome/nfp/flower/main.c in the Linux kernel before 5.3.4 allows attackers to cause a denial of service (memory consumption), aka CID-8ce39eb5a67a.
CVE-2019-19043
A memory leak in the i40e_setup_macvlans() function in drivers/net/ethernet/intel/i40e/i40e_main.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering i40e_setup_channel() failures, aka CID-27d461333459
CVE-2019-19046
** DISPUTED ** A memory leak in the __ipmi_bmc_register() function in drivers/char/ipmi/ipmi_msghandler.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering ida_simple_get() failure, aka CID-4aa7afb0ee20. NOTE: third parties dispute the relevance of this because an attacker cannot realistically control this failure at probe time.
CVE-2019-19050
A memory leak in the crypto_reportstat() function in crypto/crypto_user_stat.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering crypto_reportstat_alg() failures, aka CID-c03b04dcdba1.
CVE-2019-19053
A memory leak in the rpmsg_eptdev_write_iter() function in drivers/rpmsg/rpmsg_char.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering copy_from_iter_full() failures, aka CID-bbe692e349e2.
CVE-2019-19054
A memory leak in the cx23888_ir_probe() function in drivers/media/pci/cx23885/cx23888-ir.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering kfifo_alloc() failures, aka CID-a7b2df76b42b.
CVE-2019-19055
** DISPUTED ** A memory leak in the nl80211_get_ftm_responder_stats() function in net/wireless/nl80211.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering nl80211hdr_put() failures, aka CID-1399c59fa929. NOTE: third parties dispute the relevance of this because it occurs on a code path where a successful allocation has already occurred.
CVE-2019-19056
A memory leak in the mwifiex_pcie_alloc_cmdrsp_buf() function in drivers/net/wireless/marvell/mwifiex/pcie.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering mwifiex_map_pci_memory() failures, aka CID-db8fd2cde932.
CVE-2019-19057
Two memory leaks in the mwifiex_pcie_init_evt_ring() function in drivers/net/wireless/marvell/mwifiex/pcie.c in the Linux kernel through 5.3.11 allow attackers to cause a denial of service (memory consumption) by triggering mwifiex_map_pci_memory() failures, aka CID-d10dcb615c8e.
CVE-2019-19058
A memory leak in the alloc_sgtable() function in drivers/net/wireless/intel/iwlwifi/fw/dbg.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering alloc_page() failures, aka CID-b4b814fec1a5.
CVE-2019-19059
Multiple memory leaks in the iwl_pcie_ctxt_info_gen3_init() function in drivers/net/wireless/intel/iwlwifi/pcie/ctxt-info-gen3.c in the Linux kernel through 5.3.11 allow attackers to cause a denial of service (memory consumption) by triggering iwl_pcie_init_fw_sec() or dma_alloc_coherent() failures, aka CID-0f4f199443fa.
CVE-2019-19062
A memory leak in the crypto_report() function in crypto/crypto_user_base.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering crypto_report_alg() failures, aka CID-ffdde5932042.
CVE-2019-19063
Two memory leaks in the rtl_usb_probe() function in drivers/net/wireless/realtek/rtlwifi/usb.c in the Linux kernel through 5.3.11 allow attackers to cause a denial of service (memory consumption), aka CID-3f9361695113.
CVE-2019-19064
** DISPUTED ** A memory leak in the fsl_lpspi_probe() function in drivers/spi/spi-fsl-lpspi.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering pm_runtime_get_sync() failures, aka CID-057b8945f78f. NOTE: third parties dispute the relevance of this because an attacker cannot realistically control these failures at probe time.
CVE-2019-19066
A memory leak in the bfad_im_get_stats() function in drivers/scsi/bfa/bfad_attr.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering bfa_port_get_stats() failures, aka CID-0e62395da2bd.
CVE-2019-19068
A memory leak in the rtl8xxxu_submit_int_urb() function in drivers/net/wireless/realtek/rtl8xxxu/rtl8xxxu_core.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering usb_submit_urb() failures, aka CID-a2cdd07488e6.
CVE-2019-19070
** DISPUTED ** A memory leak in the spi_gpio_probe() function in drivers/spi/spi-gpio.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering devm_add_action_or_reset() failures, aka CID-d3b0ffa1d75d. NOTE: third parties dispute the relevance of this because the system must have already been out of memory before the probe began.
CVE-2019-19071
A memory leak in the rsi_send_beacon() function in drivers/net/wireless/rsi/rsi_91x_mgmt.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering rsi_prepare_beacon() failures, aka CID-d563131ef23c.
CVE-2019-19072
A memory leak in the predicate_parse() function in kernel/trace/trace_events_filter.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption), aka CID-96c5c6e6a5b6.
CVE-2019-19073
Memory leaks in drivers/net/wireless/ath/ath9k/htc_hst.c in the Linux kernel through 5.3.11 allow attackers to cause a denial of service (memory consumption) by triggering wait_for_completion_timeout() failures. This affects the htc_config_pipe_credits() function, the htc_setup_complete() function, and the htc_connect_service() function, aka CID-853acf7caf10
CVE-2019-19074
A memory leak in the ath9k_wmi_cmd() function in drivers/net/wireless/ath/ath9k/wmi.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption), aka CID-728c1e2a05e4.
CVE-2019-19077
A memory leak in the bnxt_re_create_srq() function in drivers/infiniband/hw/bnxt_re/ib_verbs.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering copy to udata failures, aka CID-4a9d46a9fe14.
CVE-2019-19078
A memory leak in the ath10k_usb_hif_tx_sg() function in drivers/net/wireless/ath/ath10k/usb.c in the Linux kernel through 5.3.11 allows attackers to cause a denial of service (memory consumption) by triggering usb_submit_urb() failures, aka CID-b8d17e7d93d2.
CVE-2019-19082
Memory leaks in *create_resource_pool() functions under drivers/gpu/drm/amd/display/dc in the Linux kernel through 5.3.11 allow attackers to cause a denial of service (memory consumption). This affects the dce120_create_resource_pool() function in drivers/gpu/drm/amd/display/dc/dce120/dce120_resource.c, the dce110_create_resource_pool() function in drivers/gpu/drm/amd/display/dc/dce110/dce110_resource.c, the dce100_create_resource_pool() function in drivers/gpu/drm/amd/display/dc/dce100/dce100_resource.c, the dcn10_create_resource_pool() function in drivers/gpu/drm/amd/display/dc/dcn10/dcn10_resource.c, and the dce112_create_resource_pool() function in drivers/gpu/drm/amd/display/dc/dce112/dce112_resource.c, aka CID-104c307147ad.
CVE-2020-11565
An issue was discovered in the Linux kernel through 5.6.2. mpol_parse_str in mm/mempolicy.c has a stack-based out-of-bounds write because an empty nodelist is mishandled during mount option parsing, aka CID-aa9f7d5172fa.
CVE-2019-19524
In the Linux kernel before 5.3.12, there is a use-after-free bug that can be caused by a malicious USB device in the drivers/input/ff-memless.c driver, aka CID-fa3a5a1880c9.
CVE-2019-19807
In the Linux kernel before 5.3.11, sound/core/timer.c has a use-after-free caused by erroneous code refactoring, aka CID-e7af6307a8a5. This is related to snd_timer_open and snd_timer_close_locked. The timeri variable was originally intended to be for a newly created timer instance, but was used for a different purpose after refactoring.
CVE-2019-19526
In the Linux kernel before 5.3.9, there is a use-after-free bug that can be caused by a malicious USB device in the drivers/nfc/pn533/usb.c driver, aka CID-6af3aa57a098.
CVE-2019-19532
n the Linux kernel before 5.3.9, there are multiple out-of-bounds write bugs that can be caused by a malicious USB device in the Linux kernel HID drivers, aka CID-d9d4b1e46d95. This affects drivers/hid/hid-axff.c, drivers/hid/hid-dr.c, drivers/hid/hid-emsff.c, drivers/hid/hid-gaff.c, drivers/hid/hid-holtekff.c, drivers/hid/hid-lg2ff.c, drivers/hid/hid-lg3ff.c, drivers/hid/hid-lg4ff.c, drivers/hid/hid-lgff.c, drivers/hid/hid-logitech-hidpp.c, drivers/hid/hid-microsoft.c, drivers/hid/hid-sony.c, drivers/hid/hid-tmff.c, and drivers/hid/hid-zpff.c.
CVE-2020-11609
An issue was discovered in the stv06xx subsystem in the Linux kernel before 5.6.1. drivers/media/usb/gspca/stv06xx/stv06xx.c and drivers/media/usb/gspca/stv06xx/stv06xx_pb0100.c mishandle invalid descriptors, as demonstrated by a NULL pointer dereference, aka CID-485b06aadb93.
CVE-2020-8832
The fix for the Linux kernel in Ubuntu 18.04 LTS for CVE-2019-14615 ("The Linux kernel did not properly clear data structures on context switches for certain Intel graphics processors.") was discovered to be incomplete, meaning that in versions of the kernel before 4.15.0-91.92, an attacker could use this vulnerability to expose sensitive information.
CVE-2020-2732
A flaw was discovered in the way that the KVM hypervisor handled instruction emulation for an L2 guest when nested virtualisation is enabled. Under some circumstances, an L2 guest may trick the L0 guest into accessing sensitive L1 resources that should be inaccessible to the L2 guest.