This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 ipnc-MT5 Version 2.5 question

Dear all:

I am using version 2.5 code of ipnc  from appro, it fix WAN RTSP streaming issue, but I find another issue in new release version,

when I use new cramfsImage_ipnc_dm368_2.5.0 and uImage_ipnc_dm368_2.5.0 to load into NADN flash, it can work very well in the first boot,

but when I reboot IPNC, it will show a strange error message "Error -3 while decompressing!" on terminal and can't into login page anymore

I find the  -3 error means Z_DATA_ERROR,  can anyone help me?

I try to make a new cramfs and uImage by myself, but the situation is the same, it will show the message when second boot.

Does anyone has the same issue?

My U-boot parameter and error message are as follow:

//  U-boot parameter

bootdelay=4

baudrate=115200

ethaddr=00:0C:0C:A0:05:84

bootfile=uImage_ipnc_DM368

nfshost=192.168.56.2

rootpath=/home/hirain/ipnc/target/filesys

bootcmd=nand read 0x82000000 0x700000 0xD00000;nboot 0x80700000 0 0x500000;bootm 0x80700000

bootargs=mem=46M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,14M ip=192.168.1.101:192.168.1.100:192.168.1.1:255.255.255.0:::off eth=00:0C:0C:A0:05:84

filesize=D6A000

fileaddr=82000000

ipaddr=192.168.56.103

serverip=192.168.56.2

stdin=serial

stdout=serial

stderr=serial

ver=U-Boot 1.3.4 (Apr 20 2010 - 11:42:44) DM368-IPNC-1.0.0

 

Environment size: 579/131068 bytes

 

 

//error boot message

NAND read device 0 offset 0x700000, size 0xd00000

 13631488 bytes read OK

 

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000

   Image Name   Linux-2.6.18_pro500-davinci_IPNC

   Image Type   ARM Linux Kernel Image (uncompressed)

   Data Size    1865152 Bytes =  1.8 MB

   Load Address 80008000

   Entry Point  80008000

## Booting kernel from Legacy Image at 80700000 ...

   Image Name   Linux-2.6.18_pro500-davinci_IPNC

   Image Type   ARM Linux Kernel Image (uncompressed)

   Data Size    1865152 Bytes =  1.8 MB

   Load Address 80008000

   Entry Point  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

 

Starting kernel ...

 

Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.5.0 (root@localhost.localdomain

) (gcc  4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fr

i Jan 21 163427 CST 2011

CPU ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

Machine DaVinci DM368 IPNC

Memory policy ECC disabled, Data cache writeback

DaVinci DM0365 variant 0x8

PLL0 fixedrate 24000000, commonrate 170000000, vpssrate 340000000

PLL0 vencrate_sd 75555555, ddrrate 340000000 mmcsdrate 48571428

PLL1 armrate 432000000, voicerate 20571428, vencrate_hd 27000000

CPU0 D VIVT write-back cache

CPU0 I cache 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0 D cache 8192 bytes, associativity 4, 32 byte lines, 64 sets

Built 1 zonelists.  Total pages 11776

Kernel command line mem=46M console=ttyS1,115200n8 root=devram0 rw initrd=0x8

2000000,14M ip=192.168.1.101192.168.1.100192.168.1.1255.255.255.0off eth=0

00C0CA00584

TI DaVinci EMAC kernel boot params Ethernet address 000C0CA00584

PID hash table entries 256 (order 8, 1024 bytes)

Clock event device timer0_0 configured with caps set 07

Console colour dummy device 80x30

Dentry cache hash table entries 8192 (order 3, 32768 bytes)

Inode-cache hash table entries 4096 (order 2, 16384 bytes)

Memory 46MB = 46MB total

Memory 28236KB available (3193K code, 653K data, 184K init)

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries 512

CPU Testing write buffer coherency ok

checking if image is initramfs...it isn't (bad gzip magic numbers); looks like a

n initrd

Freeing initrd memory 14336K

NET Registered protocol family 16

DaVinci 104 gpio irqs

MUX initialized GPIO20

MUX initialized I2C_SCL

Generic PHY Registered new driver

ch0 default output COMPOSITE, mode NTSC

VPBE Encoder Initialized

SCSI subsystem initialized

NET Registered protocol family 2

IP route cache hash table entries 512 (order -1, 2048 bytes)

TCP established hash table entries 2048 (order 1, 8192 bytes)

TCP bind hash table entries 1024 (order 0, 4096 bytes)

TCP Hash tables configured (established 2048 bind 1024)

TCP reno registered

VFS Disk quotas dquot_6.5.1

Dquot-cache hash table entries 1024 (order 0, 4096 bytes)

squashfs version 3.1 (20060819) Phillip Lougher

JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.

yaffs Jan 21 2011 163034 Installing.

SGI XFS with no debug enabled

Initializing Cryptographic API

io scheduler noop registered

io scheduler anticipatory registered (default)

LTT  ltt-facilities init

LTT  ltt-facility-core init in kernel

DAVINCI-WDT DaVinci Watchdog Timer heartbeat 60 sec

Serial 825016550 driver $Revision 1.90 $ 2 ports, IRQ sharing disabled

serial8250.0 ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A

serial8250.0 ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A

RAMDISK driver initialized 1 RAM disks of 32768K size 1024 blocksize

Davinci EMAC MII Bus probed

MAC address is 000C0CA00584

TI DaVinci EMAC Linux version updated 4.0

netconsole not configured, aborting

Linux video capture interface v2.00

Trying to register davinci display video device.

layer=c2c25000,layer-video_dev=c2c25160

Trying to register davinci display video device.

layer=c2dd7e00,layer-video_dev=c2dd7f60

davinci_initDaVinci V4L2 Display Driver V1.0 loaded

i2c dev entries driver

nand_davinci nand_davinci.0 Using 4-bit hardware ECC

NAND device Manufacturer ID 0xec, Chip ID 0xf1 (Samsung NAND 128MiB 3,3V 8-bi

t)

Creating 6 MTD partitions on nand_davinci.0

0x00000000-0x00300000  bootloader

0x00300000-0x00500000  params

0x00500000-0x00700000  kernel

0x00700000-0x01f00000  filesystem

0x01f00000-0x02100000  data1

0x02100000-0x08000000  data2

nand_davinci nand_davinci.0 hardware revision 2.3

musb_hdrc version 6.0, cppi-dma, peripheral, debug=0

musb_hdrc musb_hdrc No DMA interrupt line

musb_hdrc USB Peripheral mode controller at c3066000 using DMA, IRQ 12

rtc_davinci_dm365 rtc_davinci_dm365.0 rtc intf proc

rtc_davinci_dm365 rtc_davinci_dm365.0 rtc intf dev (2540)

rtc_davinci_dm365 rtc_davinci_dm365.0 rtc core registered rtc_davinci_dm365 as

 rtc0

davinci-mmc davinci-mmc.0 Supporting 4-bit mode

davinci-mmc davinci-mmc.0 Using DMA mode

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 135550

2006 UTC).

ASoC version 0.13.1

CQ0093 Voice Codec 0.1

asoc cq93vc - davinci-vcif mapping ok

ALSA device list

  #0 On-chip voice codec (cq93vc)

IPv4 over IPv4 tunneling driver

TCP bic registered

NET Registered protocol family 1

NET Registered protocol family 17

rtc_davinci_dm365 rtc_davinci_dm365.0 setting the system clock to 2000-01-01 08

0024 (946713624)

Time timer0_1 clocksource has been installed.

Clock event device timer0_0 configured with caps set 08

Switched to high resolution mode on CPU 0

IP-Config Complete

      device=eth0, addr=192.168.1.101, mask=255.255.255.0, gw=192.168.1.1,

     host=192.168.1.101, domain=, nis-domain=(none),

     bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=

RAMDISK cramfs filesystem found at block 0

RAMDISK Loading 13956KiB [1 disk] into ram disk... done.

VFS Mounted root (cramfs filesystem) readonly.

Freeing init memory 184K

INIT version 2.86 booting

0

mkdir Cannot create directory `dev.test' Read-only file system

Starting the hotplug events dispatcher udevd.

Synthesizing the initial hotplug events...done.

Waiting for dev to be fully populated...done.

0

CSL Module install successful, device major num = 253

CSL Module version 0.10.00, built on Jan 21 2011 170146

I2C Module install successful, device major num = 252

DMA Module install successful, device major num = 251

DRV Module install successful

DRV Module built on Jan 21 2011 170152

DRV EDMACC.QUEPRI  = 00000777

DRV SYSTEM.MSTPRI0 = 00550011

DRV SYSTEM.MSTPRI1 = 00000444

DRV ISP.BCR        = 00000002

DRV SYSTEM.MISC = 00000391

CMEMK module built on Jan 21 2011 at 163646

  Reference Linux version 2.6.18

  File homehiraindvsdk_2_10_01_18linuxutils_2_24_03packagestisdolinuxuti

lscmemsrcmodulecmemk.c

allocated heap buffer 0xc4000000 of size 0x5000000

CMEM Range Overlaps Kernel Physical - allowing overlap

CMEM phys_start (0x1000) overlaps kernel (0x80000000 - 0x82e00000)

cmemk initialized

EDMAK module built on Jan 21 2011 at 163650

  Reference Linux version 2.6.18

  File homehiraindvsdk_2_10_01_18linuxutils_2_24_03packagestisdolinuxuti

lsedmasrcmoduleedmak.c

IRQK module built on Jan 21 2011 at 163652

  Reference Linux version 2.6.18

  File homehiraindvsdk_2_10_01_18linuxutils_2_24_03packagestisdolinuxuti

lsirqsrcmoduleirqk.c

irqk initialized

Creat queue id0

queue id0

FileMngThread created

Creat queue id32769

queue id32769

AlramThread created

Share memory init success

Creat queue id65538

queue id65538

Creat queue id98307

queue id98307

queue id32769

IPNC_DM368_2.5.0 (root@localhost.localdomain) (gcc  4.2.0

queue id65538

 

CPU is DM368

.av_server.out DM368 NTSC TI2A AEWB 720P H264 5000000 VBR AUTO MENUOFF &

Check_device_version  DEVICE VER = 1 !!

Starting mounting local filesystems

AVSERVER UI Initializing.

DRV_SyncRst module = 47, domain = 0, state = 0

DRV_SyncRst module = 47, domain = 0, state = 3

ApproDrvInit 7

Creat queue id131076

queue id131076

 

 CLK Hz,

 ARM   Hz =  432000000

 DDR   Hz =  340000000

 VPSS  Hz =  340000000

 IMCOP Hz =  340000000

 

 [OSA_FILE ] Reading file [mntnandIMG_Paramset.bin] ... ERROR

IMAGE TUNE Paramset File is not available..... Setting DEFAULT parameter

mount none on devshm type tmpfs (rw,size=5M)

none on varrun type tmpfs (rw)

none on tmp type tmpfs (rw,sync)

Setting up networking ...rm unable to remove `etcnetworkrun' Read-only file

 system

Starting hotplug subsystem

   pci

 

CONFIGURING AVSERVER FOR DM368 .....

queue id65538

SENSOR FPS VALUE = 30

   pci      [success]

   usb

DavinciDisplay DavinciDisplay.1 Before finishing with S_FMT

layer.pix_fmt.bytesperline = 640,

 layer.pix_fmt.width = 640,

 layer.pix_fmt.height = 480,

 layer.pix_fmt.sizeimage =460800

DavinciDisplay DavinciDisplay.1 pixfmt-width = 640,

 layer-layer_info.config.line_length= 640

 

 

 FR  0 users registered from exsiting face album

IPNC_DM368_2.5.0 (root@localhost.localdomain) (gcc  4.2.0

IPNC AUTO_IRIS = 1

TI AWB PRODUCTION VERSION 1.0.0

   usb      [success]

   isapnp

   isapnp   [success]

   ide

   ide      [success]

   input

   input    [success]

   scsi

Simple mixer control 'PGA',0

  Capabilities cvolume

  Capture channels Mono

  Limits Capture 0 - 3

  Mono Capture 2 [67%]

Simple mixer control 'Mono DAC',0

  Capabilities pvolume pvolume-joined

  Playback channels Mono

  Limits Playback 0 - 63

  Mono Playback 47 [75%]

SystemInit success

Schedule manager init success

   scsi     [success]

done.

Starting portmap daemon portmap.

Starting internet superserver inetd.

io scheduler deadline registered

io scheduler cfq registered

insmod optipncmodulesi2c-emac.ko No such file or directory

 sbulla unknown partition table

Installing knfsd (copyright (C) 1996 okir@monad.swb.de).

loop loaded (max 8 devices)

tun Universal TUNTAP device driver, 1.6

tun (C) 1999-2004 Max Krasnyansky maxk@qualcomm.com

CSLIP code copyright 1989 Regents of the University of California

PPP generic driver version 2.4.2

insmod optipncmodulesnetconsole.ko No such file or directory

PPP Deflate Compression module registered

insmod optipncmodulesdavinci_emac.ko No such file or directory

insmod optipncmodulesmmc_core.ko No such file or directory

insmod optipncmodulesmmc_block.ko No such file or directory

insmod optipncmodulesdavLoading iSCSI transport class v1.1-646.inci-mmc.ko

 No such file or directory

insmod optipncmodulesusbcore.ko No such file or directory

insmod optipncmodulesmusb_hdrc.ko No such file or directory

insmod optipncmodulesusbmon.ko No such file or directory

5iscsi registered transport (tcp)

 sbulla unknown partition table

mkdosfs 3.0.6 (04 Oct 2009)

unable to get drive geometry, using default 25563

devsbulla has 255 heads and 63 sectors per track,

logical sector size is 512,

using 0xf8 media descriptor, with 1024 sectors;

file system has 2 12-bit FATs and 4 sectors per cluster.

FAT size is 1 sector, and provides 247 clusters.

Root directory contains 512 slots.

Volume ID is 42665c4f, no volume label.

queue id0

umount mntmmc not mounted

killall dhcpcd no process killed

rm cannot remove `varrundhcpcd-eth0.pid' No such file or directory

net_search_gatewayeth0, 1A8C0, 0, 1

dns=192.168.1.1

net_search_gatewayeth0, 1A8C0, 0, 1

net_search_gatewayeth0, 0, FE01A8C0, 3

dns=192.168.1Error -3 while decompressing!

.1

c03da02c(328)-c05a5000(4096)

Error -3 while decompressing!

c03da174(2584)-c05a7000(4096)

g_file_storage gadget File-backed Storage Gadget, version 28 November 2005

ERROR Module g_g_file_storage gadget Number of LUNs=1

file_storage doeg_file_storage gadget-lun0 ro=0, file devsbulla

s not exist in procmodules

system_server536[CPU#0] BUG in local_bh_enable at kernelsoftirq.c196

ApproDrvInit 3

queue id131076

queue id0

queue id32769

ApproDrvInit 9

queue id131076

Initializing...

...done initializing

ApproDrvInit 8

queue id131076

ApproDrvInit 2

queue id131076

Initializing...

...done initializing

Play this stream using the URL

        rtsp192.168.1.1688553PSIAStreamingchannels1videoCodecType=MPEG4

 

ApproDrvInit 6

queue id131076

Initializing...

...done initializing

Play this stream using the URL

        rtsp192.168.1.1688554PSIAStreamingchannels1videoCodecType=MPEG4

 

ApproDrvInit 10

queue id131076

Initializing...

...done initializing

Play this stream using the URL

        rtsp192.168.1.1688557PSIAStreamingchannels2videoCodecType=H.264

 

UDPString=uuidUpnp-TVEmulator-1_0-00_0027124105UDN

 

Initializing...

...done initializing

Play this stream using the URL

        rtsp192.168.1.1688555PSIAStreamingchannels0videoCodecType=MJPEG

 

INIT Entering runlevel 3

Upnp port is 0

UPnP Initialized OK ip=192.168.1.168, port=49152

desc_doc_url = http192.168.1.168tvdevicedesc.xml

error code = 0

device advertisement succeed.

 

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)

 

192.168.1.101 login

 

 

//////////////////////////////////////

Can anyone help me? Thanks a lot.

  • Hi,

     

    from the log it looks like 0xd00000 is not suffcient to uncompress the cramfs. PLease use higher size like 0xe00000

    PLease use these comands below doe DM368:

    tftpboot 0x80700000 uImage_ipnc_dm36x_xxx
    tftpboot 0x82000000 cramfsImage_ipnc_dm36x_xx

    nand erase 0x500000 0x1000000
    nand write 0x80700000 0x500000 0x200000
    nand write 0x82000000 0x700000 0xE00000

     

    Also, i feel your bootcmd and bootargs are as per given in User guide, please use as follows for DM368 in your case:

    setenv bootcmd 'nboot 0x80700000 0 0x500000;bootm 0x80700000'
    setenv bootargs 'mem=48M console=ttyS1,115200n8 root=/dev/mtdblock3 rootfstype=cramfs ip=192.168.1.101:192.168.1.100:192.168.1.1:255.255.255.0:::off eth=00:0C:0C:A0:05:84'

     

    Regards,

     

    Raghu



  • Dear  Raghu:

    Thanks for your help, the issue has been solved.