Part Number: AM6548
Hi, TI team
Currently, I am testing the AM65x industrial development kit.
The SDK version I use is ti-processor-sdk-linux-rt-am65xx-evm-06.02.00.81.
Based on schematic, there are 4GB memory in the AM65x industrial development kit.
I try to reduce the memory size use by OS.
My first step is modify below parameter from 32 to 16 in order to limit the totally memory size to 2GB.
Second, I export the u-boot dtsi file and replace the origin k3-am654-base-board-ddr4-1600MTs.dtsi by this file. The export file as below.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/k3_2D00_am654_2D00_base_2D00_board_2D00_ddr4_2D00_1600MTs.7z
Finally, I compile the r5 u-boot image (tiboot3.bin) and use this image to boot up the IDK.
But, boot up fail.........
The boot up log as below. There are not any message after "Starting ATF on ARM64 core...".
I guess there are other files need to patch except EMIF.
But I don't have any idea........
Could you provide some advice?
Thanks