This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: Start with J6ECO/TDA2E

Part Number: TDA2E
Other Parts Discussed in Thread: DRA726

Hello!

I have a J6ECO/TDA2E EVM CPU BOARD with a DRA726 processor. A few questions:

1. Can I use J6ECO/TDA2E with PROCESSOR_SDK_VISION? or I need another SDK.
2. If I  will use PROCESSOR_SDK_VISION, examples for my Board will be:
a) sample_app - tda2x_vm_bios_all? Are the examples suitable for J6ECO/TDA2E?
b) apps - tda2ex_vm_bios_all or still tda2xx_evm_bios_all? Are there any differences?

3. Which defines is correct for my Board SOC_TDA2XXX or SOC_DRA72x or SOC_TDA2EX in source code?
Name of board TDA2E (it is written on the EVM), but the DRA726 processor is installed. TDA2EX and DRA726 are the same? Is there a difference between them?

George