This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Max EMIF speed on DM368

Dear experts!
I'm trying to find out what maximun data transfer rate I can achive over EMIF on DM368. I need to read as fast as possible from a "black-box" device. The interface on the device can be flexible. Based on the numbers in the DM368 spec I came up with about 54MHz  in async mode. Is this close to truth? Is there any way to achieve higher speeds?

Thanks,

A.

  • Alexander,

    ~50MHz is about the maximun data transfer for EMIFA.  Peerhaps the transfer can be accomplish using another interface (i.e. usb, ethernet)

    Marcus

  • Marcus,

    first, even at 50MHz and a 16-bit bus EMIF is faster than what USB or Ethernet can provide on the DM368.

    Second, in a synchronous burst mode EMIF supposedly can work at 66MHz clock (SPRS668A, p.103). The overhead can be very low with long bursts. What limits the burst length on EMIF in a synchronous mode (when used not with OneNAND flash, but with an interface that could be optimized for speed)?

    Regards,

    A.

  • I'm still trying to figure out the fastest AEMIF speed on the DM368. Need help interpreting the data sheet (SPRS668B).

     

    Asynchronous mode.

    Table 6-22, p.101:

    EMIF read cycle = (RS + RST + RH + 3) * E >= 6 * E,

    where E = 0.5 (PLL1CSYSCLK4 period, ns) (note 1 to Table 6-21).

     

    From Tables 3-2 and 3-4 I made a conclusion that max frequency for PLL1CSYSCLK4 is 170 MHz. => E = 0.5 (1 / 170) = 2.94 ns.

    So min EMIF read cycle time is 6*2.94 = 17.64 ns <-> 56.7 MHz.

     

    Synchronous mode.

     

    Table 6-22: synchronous burst read clock = 66 MHz.

    Waveforms on p.105 show that data is read each clock cycle during the burst.

    What limits the burst length?

     

     

    Are those conclusions correct (async read rate = 56.7 * 2 = 113 MB/s, sync burst read rate = 66 * 2 = 132 MB/s)?

    Thanks,

    A.