Part Number: TMDSICE3359
Other Parts Discussed in Thread: AM3359
Tool/software: Code Composer Studio
I am using the ICEv2 (TMDSICE3359) to debug a program with an XDS100v3 probe.
If I debug without setting any GEL file, I cam load the PDK examples (and my own program) into the EMIF DDR3 RAM located in memory at 0x80000000. Notably, there does not appear to be any configuration of this DDR RAM, and yet it works.
If I set the GEL file at ccs_base/emulation/boards/ice_am3359/gel/TMDXICE3359.gel, the GEL runs OK and then the file load into DDR also works.
Why does this work at all without a GEL file to do DDR/EMIF init?