This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2E: Cascade Radar (4 AWR1243) Capture + Null (TDA2xx Only) changed ,it did'nt send data

Part Number: TDA2E
Other Parts Discussed in Thread: AWR1243

I changed the number of TX antennas 3, received antennas to 4, numradar s1, the Cascade Radar (4 AWR1243) Capture + Null (TDA2xx Only) casedoes not send data .and the Uart prints

the below information.,could you tell me why from the printed information?

10:21:54.245 [IPU1-0] 32.593973 s: Chains: Using TFDTP. Ensure using 鈥�-usetfdtp with network tools..

[IPU1-0] 32.594156 s: CAPTURE: Create in progress !!!

[IPU1-0] 32.594430 s: CAPTURE: VIP1 Slice1 PortA capture mode is [16-bit] !!!

[IPU1-0] 32.771365 s: CAPTURE: Create Done !!!

[IPU1-0] 32.771731 s: IPC_OUT_0 : Create in progress !!!

[IPU1-0] 32.772128 s: IPC_OUT_0 : Create Done !!!

[IPU1-0] 32.774903 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[IPU1-0] 32.775086 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 257856 B (251 KB)

[IPU1-0] 32.775269 s: SYSTEM: Heap = SR_OCMC @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)

10:21:54.367 [IPU1-0] 32.775391 s: SYSTEM: Heap = SR_DDR_CACHED @ 0x8a783000, Total size = 355979264 B (339 MB), Free size = 343396352 B (327 MB)

[IPU1-0] 32.775574 s: SYSTEM: Heap = SR_DDR_NON_CACHED @ 0x00000000, Total size = 0 B (0 MB), Free size = 0 B (0 MB)

[IPU1-0] 32.799213 s: CHAINS: AR12xx Starting Radar Sensor ...

[IPU1-0] 32.801256 s: CHAINS: AR12xx Starting Radar Sensor ... DONE !!!

[IPU1-0] 32.801897 s: CAPTURE: Start in progress !!!

[IPU1-0] 32.804367 s: CAPTURE: Start Done !!!

[IPU1-0] 32.806685 s:

[IPU1-0]

[IPU1-0] ====================

[IPU1-0] Chains Run-time Menu

[IPU1-0] ====================

[IPU1-0]

[IPU1-0] 0: Stop Chain

[IPU1-0]

[IPU1-0] p: Print Performance Statistics

[IPU1-0]

[IPU1-0] Enter Choice:

[IPU1-0]

[IPU1-1] 32.772463 s: IPC_IN_0 : Create in progress !!!

[IPU1-1] 32.773714 s: IPC_IN_0 : Create Done !!!

[IPU1-1] 32.774568 s: NETWORK_TX: NETWORK_TX: Server listening (port=29172) !!!

[IPU1-1] 32.775910 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[IPU1-1] 32.776093 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 655360 B (640 KB), Free size = 637592 B (622 KB)

[DSP1 ] 32.776459 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[DSP1 ] 32.776489 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)

[DSP1 ] 32.776550 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 523928 B (511 KB)

[EVE1 ] 32.777069 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[EVE1 ] 32.778198 s: SYSTEM: Heap = LOCAL_L2 @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)

[EVE1 ] 32.780333 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261792 B (255 KB)

[EVE2 ] 32.782712 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[EVE2 ] 32.783901 s: SYSTEM: Heap = LOCAL_L2 @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)

[EVE2 ] 32.785945 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261792 B (255 KB)

[EVE3 ] 32.788354 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[EVE3 ] 32.789574 s: SYSTEM: Heap = LOCAL_L2 @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)

[EVE3 ] 32.791618 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261792 B (255 KB)

[EVE4 ] 32.793997 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023

[EVE4 ] 32.795125 s: SYSTEM: Heap = LOCAL_L2 @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)

[EVE4 ] 32.797169 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 261792 B (255 KB)

10:24:23.687