Hi
As suggested by TIDL model import step, layersGroupId are set as '0 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 1 2 2 2 2 0' in ssdJacintoNetV2 network.
Which mean DSP and EVE must run alternately in one frame.
However, the buffer in tidl_OD usecase can only be passed from EVE to DSP.
Can you explain some priciples in this collabration between DSP and EVE?
Thanks
Dolby