Other Parts Discussed in Thread: TMS320C5515
Hi,
Based on the C5515 Silicon Errata, http://focus.ti.com/lit/er/sprz308a/sprz308a.pdf in advisory 2.0.9 named "USB Boot Does Not Work if the On-Chip USB_LDO Supplies Power to the USB Core" it is specified this as a workaround "For the applications that require USB boot, the USB Core (USB_VDD1P3, USB_VDDA1P3) must be powered externally".
My question, is this the only Core that should be powered directly from an external LDO or is it there anything else additionally for another Core, that is required to be powered externally in order to have succesful USB Boot?
Is the USB LDO the only LDO that is left out from the bootloader or are there more integrated LDO's that been left out not enabled and more Cores are required to be powered externally in order to perform USB Boot?
Are the ANA_LDO and DSP_LDO powered properly from the C5515 bootloader during the USB boot process or should we power the relevant Cores externally too?
Christos