This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/DRA722: DRA722/ Kernel Hangs at "Starting Kernel" when booting from eMMC

Part Number: DRA722
Other Parts Discussed in Thread: PMP

Tool/software: TI C/C++ Compiler

Hi,

Using Android 6AO.1.1.

We have DRA722  based custom board. 

We would face a booting issue while we bring up our custom board, with prebuild image the Kernel Hangs at "Starting Kernel" when booting from eMMC.

but with when booting from sdcrard the kernel started well (with kernel panic due to HW definition) .

Here the uboot logs :

______________________________________
U-Boot 2016.05 (Apr 23 2020 - 11:58:39 +0200)
CPU  : DRA722-GP ES2.0
Model: TI DRA722
Board: DRA72x EVM REV 831
DRAM:  2 GiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
board_late_init:
board_ti_get_rev: version=831
SCSI:  SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot:  0
WARNING: Could not determine device tree to use
MMC: no card present
MMC: no card present
MMC: no card present
switch to partitions #0, OK
mmc1(part 0) is current device
MMC read: dev # 1, block # 5376, count 512 ... 512 blocks read: OK
MMC read: dev # 1, block # 101152, count 61440 ... 61440 blocks read: OK
Booting from eMMC ...
## Booting Android Image at 0x82000000 ...
Kernel load addr 0x80008000 size 8165 KiB
Kernel command line: buildvariant=userdebug
RAM disk load addr 0x83000000 size 2113 KiB
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Kernel Image ... OK
   Loading Ramdisk to 8fdef000, end 8ffff338 ... OK
   Loading Device Tree to 8fdd4000, end 8fdeed2b ... OK
Using machid 0xfe6 from environment
Starting kernel ...
______________________________________

the emmc flash Ok and we can list partitions and dump it from uboot: 

=> ext2ls mmc 1:11
<DIR>       4096 .
<DIR>       4096 ..
<DIR>       4096 benchmarktest
<DIR>       4096 lost+found
<DIR>       4096 nativetest
and here the mmc info result :
=> mmcinfo
Device: OMAP SD/MMC
Manufacturer ID: 13
OEM: 14e
Name: S0J35
Tran Speed: 200000000
Rd Block Len: 512
MMC version 5.1
High Capacity: Yes
Capacity: 7.3 GiB
Bus Width: 8-bit
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 7.3 GiB WRREL
Boot Capacity: 31.5 MiB ENH
RPMB Capacity: 4 MiB ENH
 Please do you know what are the possible root causes ? (why it boots from sd and Kernel Hangs at "Starting Kernel" when booting from eMMC ) ?
Regards,
Chokri

  • Hi,

    Can you make sure you are using the same dtb and kernel binary for eMMC and SD card?
    Also try enabling earlyprintk in kernel to get some additional logs.

    Regards,
    Vishal

  • Hi Vishal,

    By earlyprintk to cmdline :

    Booting from mmc0 ...

    Kernel image @ 0x82000000 [ 0x000000 - 0x363750 ]
    ## Flattened Device Tree blob at 88000000
    Booting using the fdt blob at 0x88000000
    Loading Device Tree to 8ffe3000, end 8ffff2a4 ... OK

    Starting kernel ...

    [ 0.000000] Booting Linux on physical CPU 0x0
    [ 0.000000] Initializing cgroup subsys cpuset
    [ 0.000000] Initializing cgroup subsys cpu
    [ 0.000000] Initializing cgroup subsys cpuacct
    [ 0.000000] Linux version 4.4.84-g742f84423d (tiiappadmin@swubn03) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Th
    u Jan 18 05:02:56 IST 2018
    [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [ 0.000000] Machine model: TI DRA722
    [ 0.000000] bootconsole [earlycon0] enabled
    [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
    [ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
    [ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
    [ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [ 0.000000] cma: Reserved 128 MiB at 0x00000000b0000000
    [ 0.000000] Forcing write-allocate cache policy for SMP
    [ 0.000000] Memory policy: Data cache writealloc
    [ 0.000000] OMAP4: Map 0x00000000fed00000 to fe600000 for dram barrier
    [ 0.000000] DRA722 ES2.0
    [ 0.000000] PERCPU: Embedded 11 pages/cpu @eed62000 s14912 r8192 d21952 u45056
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 516416
    [ 0.000000] Kernel command line: console=ttyO0,115200n8 elevator=noop root=PARTUUID=c35aae51-02 rw rootwait earlyprintk fixrtc omapdrm.num_
    crtc=2 consoleblank=0 cma=128M@0xB0000000 rootfstype=ext4 snd.slots_reserved=1,1
    [ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [ 0.000000] Memory: 1755896K/2072576K available (6615K kernel code, 319K rwdata, 2456K rodata, 340K init, 290K bss, 29960K reserved, 286720
    K cma-reserved, 1159168K highmem)
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
    [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
    [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
    [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc08e402c (9073 kB)
    [ 0.000000] .init : 0xc08e5000 - 0xc093a000 ( 340 kB)
    [ 0.000000] .data : 0xc093a000 - 0xc0989ee0 ( 320 kB)
    [ 0.000000] .bss : 0xc098b000 - 0xc09d3800 ( 290 kB)
    [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [ 0.000000] Preemptible hierarchical RCU implementation.
    [ 0.000000] Build-time adjustment of leaf fanout to 32.
    [ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
    [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
    [ 0.000000] NR_IRQS:16 nr_irqs:16 16
    [ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
    [ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
    [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
    [ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [ 0.008312] Switching to timer-based delay loop, resolution 162ns
    [ 0.014973] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
    [ 0.025240] OMAP clocksource: 32k_counter at 32768 Hz
    [ 0.030983] Console: colour dummy device 80x30
    [ 0.035642] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [ 0.042441] This ensures that you still see kernel messages. Please
    [ 0.048956] update your kernel commandline.
    [ 0.053345] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [ 0.063981] pid_max: default: 32768 minimum: 301
    [ 0.068902] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.075789] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.083645] Initializing cgroup subsys io
    [ 0.087870] Initializing cgroup subsys memory
    [ 0.092446] Initializing cgroup subsys devices
    [ 0.097093] Initializing cgroup subsys freezer
    [ 0.101751] Initializing cgroup subsys perf_event
    [ 0.106669] Initializing cgroup subsys pids
    [ 0.111063] CPU: Testing write buffer coherency: ok
    [ 0.116359] /cpus/cpu@0 missing clock-frequency property
    [ 0.121898] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [ 0.127835] Setting up static identity map for 0x80008380 - 0x800083e0
    [ 0.178055] Brought up 1 CPUs
    [ 0.181189] SMP: Total of 1 processors activated (12.29 BogoMIPS).
    [ 0.187620] CPU: All CPU(s) started in HYP mode.
    [ 0.192456] CPU: Virtualization extensions available.
    [ 0.198036] devtmpfs: initialized
    [ 0.232698] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [ 0.241630] omap_hwmod: l3_main_2 using broken dt data from ocp
    [ 0.444569] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
    [ 0.452165] pgd = c0003000
    [ 0.455026] [00000000] *pgd=80000080004003, *pmd=00000000
    [ 0.460663] Internal error: : 1211 [#1] PREEMPT SMP ARM
    [ 0.466111] Modules linked in:
    [ 0.469338] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.4.84-g742f84423d #1
    [ 0.476575] Hardware name: Generic DRA72X (Flattened Device Tree)
    [ 0.482921] task: ee88c000 ti: ee882000 task.ti: ee882000
    [ 0.488553] PC is at _enable_sysc+0x4c/0x230
    [ 0.493020] LR is at _enable_sysc+0x38/0x230
    [ 0.497493] pc : [<c0024d14>] lr : [<c0024d00>] psr: 40000013
    [ 0.497493] sp : ee883e30 ip : ee883e30 fp : ee883e5c
    [ 0.509455] r10: 00000000 r9 : c08e5600 r8 : 000000aa
    [ 0.514900] r7 : c0947e18 r6 : c098b610 r5 : 00000000 r4 : c09478e0
    [ 0.521685] r3 : c0947968 r2 : 00000002 r1 : c0947968 r0 : c09478e0
    [ 0.528469] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
    [ 0.536057] Control: 30c5387d Table: 80003000 DAC: fffffffd
    [ 0.542044] Process swapper/0 (pid: 1, stack limit = 0xee882210)
    [ 0.548295] Stack: (0xee883e30 to 0xee884000)
    [ 0.552850] 3e20: c002bf1c c067c1a0 ee883e5c ee883e48
    [ 0.561336] 3e40: c002dba4 c09478e0 00000000 c098b610 ee883e84 ee883e60 c002509c c0024cd4
    [ 0.569815] 3e60: ee883e84 ee883e70 c09478e0 00000002 c094792c ee9a95c0 ee883eb4 ee883e88
    [ 0.578300] 3e80: c08f1b04 c0024f04 c08f2344 c09478e0 c0941b78 0000000c ee9a95c0 c09478e0
    [ 0.586779] 3ea0: c0941b78 c093f6f0 ee883ecc ee883eb8 c08f23c0 c08f1a44 c093f6f0 c08f2344
    [ 0.595265] 3ec0: ee883f4c ee883ed0 c000982c c08f2350 ee883ef4 ee883ee0 c004f91c c02b90fc
    [ 0.603747] 3ee0: effff700 c069ddbc ee883f4c ee883ef8 c004fb10 c004f910 ee883f34 c08186c8
    [ 0.612230] 3f00: c0818714 c0817f34 00000001 00000001 00000000 c08e1de8 c0895774 00000000
    [ 0.620705] 3f20: 00000478 c098b000 c098b000 c0934280 c0926820 000000aa c08e5600 00000002
    [ 0.629188] 3f40: ee883f94 ee883f50 c08e5f68 c00097a0 00000001 00000001 00000000 c08e5600
    [ 0.637668] 3f60: 00000000 c08e1de8 00000000 c098b000 c0677548 00000000 00000000 00000000
    [ 0.646153] 3f80: 00000000 00000000 ee883fac ee883f98 c0677560 c08e5da0 00000000 c0677548
    [ 0.654634] 3fa0: 00000000 ee883fb0 c000fb88 c0677554 00000000 00000000 00000000 00000000
    [ 0.663117] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 0.671601] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
    [ 0.680077] Backtrace:
    [ 0.682680] [<c0024cc8>] (_enable_sysc) from [<c002509c>] (_enable+0x1a4/0x2d8)
    [ 0.690264] r6:c098b610 r5:00000000 r4:c09478e0
    [ 0.695105] [<c0024ef8>] (_enable) from [<c08f1b04>] (_setup.part.15+0xcc/0x3fc)
    [ 0.702785] r7:ee9a95c0 r6:c094792c r5:00000002 r4:c09478e0
    [ 0.708692] [<c08f1a38>] (_setup.part.15) from [<c08f23c0>] (__omap_hwmod_setup_all+0x7c/0x98)
    [ 0.717617] r6:c093f6f0 r5:c0941b78 r4:c09478e0
    [ 0.722455] [<c08f2344>] (__omap_hwmod_setup_all) from [<c000982c>] (do_one_initcall+0x98/0x1e4)
    [ 0.731555] r5:c08f2344 r4:c093f6f0
    [ 0.735320] [<c0009794>] (do_one_initcall) from [<c08e5f68>] (kernel_init_freeable+0x1d4/0x268)
    [ 0.744332] r10:00000002 r9:c08e5600 r8:000000aa r7:c0926820 r6:c0934280 r5:c098b000
    [ 0.752470] r4:c098b000
    [ 0.755165] [<c08e5d94>] (kernel_init_freeable) from [<c0677560>] (kernel_init+0x18/0xf4)
    [ 0.763640] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0677548
    [ 0.771778] r4:c098b000
    [ 0.774472] [<c0677548>] (kernel_init) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
    [ 0.782331] r5:c0677548 r4:00000000
    [ 0.786093] Code: e3130080 1a000061 e5943004 e1a00004 (e5942058)
    [ 0.792451] ---[ end trace 8355a4abc64bbdac ]---
    [ 0.797310] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
    [ 0.797310]
    [ 0.806868] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
    [ 0.806868]

    CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7.1 | VT102 | Offline | ttyUSB0

  • Hi,

    This doesn't look like emmc boot issue. Kernel boot has started.

    Are you sure the kernel image flashed to eMMC is the correct one? Is this the same kernel that's working on SD card boot?

    Version info from your log below. This looks like a Kernel built from TI servers.

    [ 0.000000] Linux version 4.4.84-g742f84423d (tiiappadmin@swubn03) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Thu Jan 18 05:02:56 IST 2018


    Regards,
    Vishal

  • Hi Vishal,

    Yes the last log is for boot form sd, 

    Here the log from emmc :

    Starting kernel ...

    [ 0.000000] Booting Linux on physical CPU 0x0
    [ 0.000000] Initializing cgroup subsys cpuset
    [ 0.000000] Initializing cgroup subsys cpu
    [ 0.000000] Initializing cgroup subsys cpuacct
    [ 0.000000] Linux version 4.4.117 (actia@actia-P5K-Premium) (gcc version 4.9.x 20150123 (prereleas0
    [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [ 0.000000] Machine model: TI DRA722
    [ 0.000000] bootconsole [earlycon0] enabled
    [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
    [ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
    [ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
    [ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [ 0.000000] cma: Reserved 380 MiB at 0x00000000e7000000
    [ 0.000000] Forcing write-allocate cache policy for SMP
    [ 0.000000] Memory policy: Data cache writealloc
    [ 0.000000] OMAP4: Map 0x00000000fed00000 to fe600000 for dram barrier
    [ 0.000000] DRA722 ES2.0
    [ 0.000000] PERCPU: Embedded 12 pages/cpu @eed62000 s19968 r8192 d20992 u49152
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 516416
    [ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rw init=/init rootfstype=ext4 rootwait earlypg
    [ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [ 0.000000] Memory: 1488028K/2072576K available (10240K kernel code, 665K rwdata, 3284K rodata, 20)
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
    [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
    [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
    [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc0c00000 (12256 kB)
    [ 0.000000] .init : 0xc1000000 - 0xc1200000 (2048 kB)
    [ 0.000000] .data : 0xc1200000 - 0xc12a66dc ( 666 kB)
    [ 0.000000] .bss : 0xc12a66dc - 0xc13507d8 ( 681 kB)
    [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [ 0.000000] Preemptible hierarchical RCU implementation.
    [ 0.000000] Build-time adjustment of leaf fanout to 32.
    [ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
    [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
    [ 0.000000] NR_IRQS:16 nr_irqs:16 16
    [ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
    [ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
    [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idls
    [ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [ 0.008311] Switching to timer-based delay loop, resolution 162ns
    [ 0.014942] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 583270s
    [ 0.025204] OMAP clocksource: 32k_counter at 32768 Hz
    [ 0.030877] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoM)
    [ 0.041515] pid_max: default: 32768 minimum: 301
    [ 0.046407] Security Framework initialized
    [ 0.050696] SELinux: Initializing.
    [ 0.054442] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.061317] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.069215] Initializing cgroup subsys io
    [ 0.073428] Initializing cgroup subsys memory
    [ 0.078003] Initializing cgroup subsys devices
    [ 0.082673] Initializing cgroup subsys freezer
    [ 0.087325] Initializing cgroup subsys perf_event
    [ 0.092240] Initializing cgroup subsys pids
    [ 0.096661] CPU: Testing write buffer coherency: ok
    [ 0.101988] /cpus/cpu@0 missing clock-frequency property
    [ 0.107553] CPU0: update cpu_capacity 1024
    [ 0.111841] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [ 0.117790] Setting up static identity map for 0x80200000 - 0x80200060
    [ 0.168079] Brought up 1 CPUs
    [ 0.171213] SMP: Total of 1 processors activated (12.29 BogoMIPS).
    [ 0.177643] CPU: All CPU(s) started in HYP mode.
    [ 0.182482] CPU: Virtualization extensions available.
    [ 0.187778] CPU0: update max cpu_capacity 1024
    [ 0.227589] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [ 0.236571] omap_hwmod: l3_main_2 using broken dt data from ocp
    [ 0.381631] omap_hwmod: dss_dispc: _wait_target_ready failed: -16
    [ 0.387998] omap_hwmod: dss_dispc: cannot be enabled for reset (3)
    [ 0.397008] omap_hwmod: dss_hdmi: _wait_target_ready failed: -16
    [ 0.403275] omap_hwmod: dss_hdmi: cannot be enabled for reset (3)
    [ 0.477394] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
    [ 0.484985] pgd = c0003000
    [ 0.487847] [00000000] *pgd=80000080004003, *pmd=00000000
    [ 0.493489] Internal error: : 1211 [#1] PREEMPT SMP ARM
    [ 0.498936] Modules linked in:
    [ 0.502163] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.4.117 #5
    [ 0.508412] Hardware name: Generic DRA72X (Flattened Device Tree)
    [ 0.514756] task: ee8d4000 task.stack: ee8d8000
    [ 0.519499] PC is at _enable_sysc+0x5c/0x250
    [ 0.523968] LR is at _enable_sysc+0x48/0x250
    [ 0.528436] pc : [<c021fba0>] lr : [<c021fb8c>] psr: 60000013
    [ 0.528436] sp : ee8d9e08 ip : ee8d9e08 fp : ee8d9e34
    [ 0.540396] r10: c120394c r9 : ee9f2880 r8 : c120bd68
    [ 0.545844] r7 : c1214b90 r6 : c12a8638 r5 : c120394c r4 : c1214658
    [ 0.552629] r3 : c12146e0 r2 : dc8ba675 r1 : c12146e0 r0 : c1214658
    [ 0.559424] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
    [ 0.567014] Control: 30c5387d Table: 80003000 DAC: fffffffd
    [ 0.572998]
    [ 0.572998] PC: 0xc021fb20:
    [ 0.577551] fb20 e3001179 e5953000 e34c00e2 e34c20e2 eb004908 e5953004 e5933004 e1d311d5
    [ 0.586062] fb40 eaffffd2 e1a0c00d e92dd8f0 e24cb004 e24dd010 e5903004 e303594c e1a04000
    [ 0.594569] fb60 e34c5120 e5933004 e5952000 e3530000 e50b2020 0a000052 e5903074 e3130080
    [ 0.603073] fb80 1a00006c e1a00004 ebfffb19 e5943074 e3130080 1a000064 e5943004 e1a00004
    [ 0.611578] fba0 e5942058 e5933004 e50b2024 e5d3600c ebfffd8c e3160020 e1a07000 0a00001a
    [ 0.620082] fbc0 e5942074 e3013001 e0033002 e24b2024 e3530000 13a01002 1a000007 e3160004
    [ 0.628583] fbe0 1a000056 e5943004 e5933004 e5d33015 e3130008 13a01008 03a01004 e3570000
    [ 0.637085] fc00 0a000007 e5d7300a e3130020 0a000004 e5943004 e5933004 e5d33015 e313000c
    [ 0.645589]
    [ 0.645589] LR: 0xc021fb0c:
    [ 0.650147] fb0c e89da830 e3e00015 e89da830 e30606c0 e3062744 e3001179 e5953000 e34c00e2
    [ 0.658651] fb2c e34c20e2 eb004908 e5953004 e5933004 e1d311d5 eaffffd2 e1a0c00d e92dd8f0
    [ 0.667158] fb4c e24cb004 e24dd010 e5903004 e303594c e1a04000 e34c5120 e5933004 e5952000
    [ 0.675661] fb6c e3530000 e50b2020 0a000052 e5903074 e3130080 1a00006c e1a00004 ebfffb19
    [ 0.684167] fb8c e5943074 e3130080 1a000064 e5943004 e1a00004 e5942058 e5933004 e50b2024
    [ 0.692675] fbac e5d3600c ebfffd8c e3160020 e1a07000 0a00001a e5942074 e3013001 e0033002
    [ 0.701176] fbcc e24b2024 e3530000 13a01002 1a000007 e3160004 1a000056 e5943004 e5933004
    [ 0.709681] fbec e5d33015 e3130008 13a01008 03a01004 e3570000 0a000007 e5d7300a e3130020
    [ 0.718186]
    [ 0.718186] SP: 0xee8d9d88:
    [ 0.722741] 9d88 c0586364 dc8ba675 c021fba0 60000013 ffffffff ee8d9dec c120bd68 ee9f2880
    [ 0.731247] 9da8 ee8d9e34 ee8d9db8 c020d498 c0201278 c1214658 c12146e0 dc8ba675 c12146e0
    [ 0.739751] 9dc8 c1214658 c120394c c12a8638 c1214b90 c120bd68 ee9f2880 c120394c ee8d9e34
    [ 0.748254] 9de8 ee8d9e08 ee8d9e08 c021fb8c c021fba0 60000013 ffffffff c021fb8c c021e800
    [ 0.756757] 9e08 c0227854 c0bf8a3c ee8d9e34 dc8ba675 c1214658 00000000 c12a8638 c1214b90
    [ 0.765261] 9e28 ee8d9e5c ee8d9e38 c021ff38 c021fb50 ee8d9e5c ee8d9e48 c1214658 00000001
    [ 0.773763] 9e48 c120394c c12146a4 ee8d9e9c ee8d9e60 c100f5b4 c021fda0 ee8d9eb0 00000000
    [ 0.782261] 9e68 eedb1dcc 0000000c c1080002 dc8ba675 c120e8d0 c1214658 c120e8d0 c100fce8
    [ 0.790766]
    [ 0.790766] IP: 0xee8d9d88:
    [ 0.795321] 9d88 c0586364 dc8ba675 c021fba0 60000013 ffffffff ee8d9dec c120bd68 ee9f2880
    [ 0.803825] 9da8 ee8d9e34 ee8d9db8 c020d498 c0201278 c1214658 c12146e0 dc8ba675 c12146e0
    [ 0.812327] 9dc8 c1214658 c120394c c12a8638 c1214b90 c120bd68 ee9f2880 c120394c ee8d9e34
    [ 0.820827] 9de8 ee8d9e08 ee8d9e08 c021fb8c c021fba0 60000013 ffffffff c021fb8c c021e800
    [ 0.829331] 9e08 c0227854 c0bf8a3c ee8d9e34 dc8ba675 c1214658 00000000 c12a8638 c1214b90
    [ 0.837836] 9e28 ee8d9e5c ee8d9e38 c021ff38 c021fb50 ee8d9e5c ee8d9e48 c1214658 00000001
    [ 0.846337] 9e48 c120394c c12146a4 ee8d9e9c ee8d9e60 c100f5b4 c021fda0 ee8d9eb0 00000000
    [ 0.854841] 9e68 eedb1dcc 0000000c c1080002 dc8ba675 c120e8d0 c1214658 c120e8d0 c100fce8
    [ 0.863347]
    [ 0.863347] FP: 0xee8d9db4:
    [ 0.867903] 9db4 c0201278 c1214658 c12146e0 dc8ba675 c12146e0 c1214658 c120394c c12a8638
    [ 0.876406] 9dd4 c1214b90 c120bd68 ee9f2880 c120394c ee8d9e34 ee8d9e08 ee8d9e08 c021fb8c
    [ 0.884907] 9df4 c021fba0 60000013 ffffffff c021fb8c c021e800 c0227854 c0bf8a3c ee8d9e34
    [ 0.893409] 9e14 dc8ba675 c1214658 00000000 c12a8638 c1214b90 ee8d9e5c ee8d9e38 c021ff38
    [ 0.901914] 9e34 c021fb50 ee8d9e5c ee8d9e48 c1214658 00000001 c120394c c12146a4 ee8d9e9c
    [ 0.910418] 9e54 ee8d9e60 c100f5b4 c021fda0 ee8d9eb0 00000000 eedb1dcc 0000000c c1080002
    [ 0.918923] 9e74 dc8ba675 c120e8d0 c1214658 c120e8d0 c100fce8 00000000 c120bd68 ee8d9eb4
    [ 0.927425] 9e94 ee8d9ea0 c100fd6c c100f4e0 00000001 c120bd68 ee8d9f44 ee8d9eb8 c0201864
    [ 0.935931]
    [ 0.935931] R0: 0xc12145d8:
    [ 0.940484] 45d8 c1211178 c12145dc c12145dc eed70ab8 eed70ab8 00000000 00000000 fc141100
    [ 0.948988] 45f8 00010001 c1214530 c121477c c1212324 00000000 00000003 00000001 02000100
    [ 0.957492] 4618 00000505 00000000 c0e28944 c1214640 00000000 00000000 00000000 00000000
    [ 0.965999] 4638 00000000 00000000 00000000 00000000 00000000 00000060 c120eba4 0000ff00
    [ 0.974506] 4658 c0e2895c c12146e0 00000000 00000000 00000000 00000000 00000000 00000004
    [ 0.983000] 4678 00040000 00000000 00000200 00000001 c0e285a0 ee9f9280 00000000 c0e28390
    [ 0.991503] 4698 c1210f68 c121469c c121469c effff890 effff890 00000000 00000000 fa838000
    [ 1.000008] 46b8 00010001 c120e8d0 c12133ec c1212360 00000000 00000000 00000000 02000100
    [ 1.008511]
    [ 1.008511] R1: 0xc1214660:
    [ 1.013063] 4660 00000000 00000000 00000000 00000000 00000000 00000004 00040000 00000000
    [ 1.021567] 4680 00000200 00000001 c0e285a0 ee9f9280 00000000 c0e28390 c1210f68 c121469c
    [ 1.030072] 46a0 c121469c effff890 effff890 00000000 00000000 fa838000 00010001 c120e8d0
    [ 1.038575] 46c0 c12133ec c1212360 00000000 00000000 00000000 02000100 00000504 00000000
    [ 1.047075] 46e0 c0e2895c c1214700 00000000 00000000 00000000 00000000 c0222688 c022263c
    [ 1.055580] 4700 00000000 00000078 00000000 00000020 c120eb9c 00000f00 c0e28964 c12147a0
    [ 1.064081] 4720 00000000 00000000 00000000 00000000 00000000 00000138 013c0000 00000000
    [ 1.072588] 4740 00000200 00000001 c0e2896c ee9f7c40 00000000 c0e28448 c1211298 c121475c
    [ 1.081095]
    [ 1.081095] R2: 0xdc8ba5f5:
    [ 1.085646] a5f4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.094151] a614 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.102650] a634 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.111156] a654 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.119661] a674 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.128163] a694 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.136665] a6b4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.145172] a6d4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.153679] a6f4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.162182]
    [ 1.162182] R3: 0xc1214660:
    [ 1.166738] 4660 00000000 00000000 00000000 00000000 00000000 00000004 00040000 00000000
    [ 1.175243] 4680 00000200 00000001 c0e285a0 ee9f9280 00000000 c0e28390 c1210f68 c121469c
    [ 1.183747] 46a0 c121469c effff890 effff890 00000000 00000000 fa838000 00010001 c120e8d0
    [ 1.192252] 46c0 c12133ec c1212360 00000000 00000000 00000000 02000100 00000504 00000000
    [ 1.200754] 46e0 c0e2895c c1214700 00000000 00000000 00000000 00000000 c0222688 c022263c
    [ 1.209251] 4700 00000000 00000078 00000000 00000020 c120eb9c 00000f00 c0e28964 c12147a0
    [ 1.217755] 4720 00000000 00000000 00000000 00000000 00000000 00000138 013c0000 00000000
    [ 1.226257] 4740 00000200 00000001 c0e2896c ee9f7c40 00000000 c0e28448 c1211298 c121475c
    [ 1.234761]
    [ 1.234761] R4: 0xc12145d8:
    [ 1.239317] 45d8 c1211178 c12145dc c12145dc eed70ab8 eed70ab8 00000000 00000000 fc141100
    [ 1.247820] 45f8 00010001 c1214530 c121477c c1212324 00000000 00000003 00000001 02000100
    [ 1.256319] 4618 00000505 00000000 c0e28944 c1214640 00000000 00000000 00000000 00000000
    [ 1.264823] 4638 00000000 00000000 00000000 00000000 00000000 00000060 c120eba4 0000ff00
    [ 1.273321] 4658 c0e2895c c12146e0 00000000 00000000 00000000 00000000 00000000 00000004
    [ 1.281830] 4678 00040000 00000000 00000200 00000001 c0e285a0 ee9f9280 00000000 c0e28390
    [ 1.290332] 4698 c1210f68 c121469c c121469c effff890 effff890 00000000 00000000 fa838000
    [ 1.298841] 46b8 00010001 c120e8d0 c12133ec c1212360 00000000 00000000 00000000 02000100
    [ 1.307346]
    [ 1.307346] R5: 0xc12038cc:
    [ 1.311901] 38cc 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.320408] 38ec 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.328910] 390c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.337416] 392c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000001
    [ 1.345922] 394c dc8ba675 003fb0d6 00000000 00000009 c021aa00 c021aa20 c021b430 c021b434
    [ 1.354427] 396c c0200044 c021b460 c021b46c c021b3e0 c021b3f8 00000024 c021b4b0 c021b4e0
    [ 1.362929] 398c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.371431] 39ac 00000000 c021b364 c021b39c 90f00000 c021ad74 c021ad30 00000022 ffffffff
    [ 1.379937]
    [ 1.379937] R6: 0xc12a85b8:
    [ 1.384491] 85b8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.392999] 85d8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.401503] 85f8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.410004] 8618 00000000 005dcdd5 ee8915c0 00000000 00000000 00000000 00000000 00000000
    [ 1.418508] 8638 c1214b90 00000000 c021f0a8 c021f758 c021f2e8 c021f068 c021efe0 c021efa0
    [ 1.427011] 8658 c021f29c c021f238 c021e920 00000001 eed701c0 01140114 00000004 00000000
    [ 1.435514] 8678 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.444017] 8698 fee00000 00000000 fe600000 00000000 00100000 00000000 fed00000 00000000
    [ 1.452523]
    [ 1.452523] R7: 0xc1214b10:
    [ 1.457077] 4b10 c1211178 c1214b14 c1214b14 eed709e0 eed709e0 00000000 00000011 fc080000
    [ 1.465577] 4b30 00010001 c1214aac c1214c9c c121247c 00000000 00000000 00000000 02000100
    [ 1.474085] 4b50 00000505 00000000 c0e289c4 c1214b78 00000000 00000000 00000000 00000000
    [ 1.482592] 4b70 00000000 00000000 00000000 00000010 00000014 000000a3 c120ebac 00000700
    [ 1.491098] 4b90 c0e25eb0 c1214c18 00000000 00000000 00000000 00000000 00000000 00000020
    [ 1.499603] 4bb0 00240000 00000000 00000000 00000001 c0e289cc ee891440 00000000 c0e276d8
    [ 1.508109] 4bd0 c12110b8 eed7020c eed7020c eed709c8 eed709c8 00000000 00000000 00000000
    [ 1.516611] 4bf0 00010001 c12182e4 c121836c c1212498 00000000 0000000c 00000000 04000101
    [ 1.525117]
    [ 1.525117] R8: 0xc120bce8:
    [ 1.529674] bce8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.538179] bd08 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.546679] bd28 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.555184] bd48 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.563690] bd68 c120bd68 c120bd68 00000001 c0e205e8 c0e205f0 effff53f 00000000 00000000
    [ 1.572197] bd88 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.580701] bda8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.589207] bdc8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.597713]
    [ 1.597713] R9: 0xee9f2800:
    [ 1.602265] 2800 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.610773] 2820 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.619277] 2840 00000001 00000000 ee8f4b10 00000000 00000000 ffffffff ffffffff 0000000b
    [ 1.627787] 2860 c121aba8 00000000 eed5e7a4 ffffffff ffffffff ffffffff ffffffff ffffffff
    [ 1.636286] 2880 ee835780 00000000 c0e28518 00000000 ffffffff ee891494 ee9f28d4 00000000
    [ 1.644789] 28a0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.653293] 28c0 ee835780 00000000 c0e28518 00000000 ffffffff ee9f2894 ee9f2914 00000000
    [ 1.661795] 28e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.670300]
    [ 1.670300] R10: 0xc12038cc:
    [ 1.674948] 38cc 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.683451] 38ec 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.691952] 390c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.700456] 392c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000001
    [ 1.708962] 394c dc8ba675 003fb0d6 00000000 00000009 c021aa00 c021aa20 c021b430 c021b434
    [ 1.717467] 396c c0200044 c021b460 c021b46c c021b3e0 c021b3f8 00000024 c021b4b0 c021b4e0
    [ 1.725969] 398c 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.734472] 39ac 00000000 c021b364 c021b39c 90f00000 c021ad74 c021ad30 00000022 ffffffff
    [ 1.742985] Process swapper/0 (pid: 1, stack limit = 0xee8d8210)
    [ 1.749240] Stack: (0xee8d9e08 to 0xee8da000)
    [ 1.753803] 9e00: c0227854 c0bf8a3c ee8d9e34 dc8ba675 c1214658 00000000
    [ 1.762287] 9e20: c12a8638 c1214b90 ee8d9e5c ee8d9e38 c021ff38 c021fb50 ee8d9e5c ee8d9e48
    [ 1.770771] 9e40: c1214658 00000001 c120394c c12146a4 ee8d9e9c ee8d9e60 c100f5b4 c021fda0
    [ 1.779256] 9e60: ee8d9eb0 00000000 eedb1dcc 0000000c c1080002 dc8ba675 c120e8d0 c1214658
    [ 1.787742] 9e80: c120e8d0 c100fce8 00000000 c120bd68 ee8d9eb4 ee8d9ea0 c100fd6c c100f4e0
    [ 1.796230] 9ea0: 00000001 c120bd68 ee8d9f44 ee8d9eb8 c0201864 c100fcf4 ee8d9ee4 ee8d9ec8
    [ 1.804715] 9ec0: c03f5b28 ffffffed c120394c ee9f3b80 ee8d9efc ee8d9e00 c100071c c0592258
    [ 1.813197] 9ee0: 00000000 c0f34624 c0c27f50 effff6cc ee8d9f44 ee8d9f00 c02525e8 c100070c
    [ 1.821679] 9f00: 00000001 00000001 00000000 c0f32f2c c0e205b0 dc8ba675 00008000 00000001
    [ 1.830159] 9f20: c1088d00 c12a8000 c12a8000 c1079820 c1000700 c107983c ee8d9f94 ee8d9f48
    [ 1.838644] 9f40: c10010b4 c02017c8 00000001 00000001 00000000 c1000700 00000126 c120394c
    [ 1.847131] 9f60: ffffffff dc8ba675 ffffffff 00000000 c0bf31ec 00000000 00000000 00000000
    [ 1.855617] 9f80: 00000000 00000000 ee8d9fac ee8d9f98 c0bf31fc c1000ec8 00000000 c0bf31ec
    [ 1.864101] 9fa0: 00000000 ee8d9fb0 c02080a0 c0bf31f8 00000000 00000000 00000000 00000000
    [ 1.872579] 9fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [ 1.881067] 9fe0: 00000000 00000000 00000000 00000000 00000013 00000000 ffffffff ffffffff
    [ 1.889545] Backtrace:
    [ 1.892147] [<c021fb44>] (_enable_sysc) from [<c021ff38>] (_enable+0x1a4/0x2d8)
    [ 1.899736] r7:c1214b90 r6:c12a8638 r5:00000000 r4:c1214658
    [ 1.905651] [<c021fd94>] (_enable) from [<c100f5b4>] (_setup.part.14+0xe0/0x498)
    [ 1.913325] r7:c12146a4 r6:c120394c r5:00000001 r4:c1214658
    [ 1.919231] [<c100f4d4>] (_setup.part.14) from [<c100fd6c>] (__omap_hwmod_setup_all+0x84/0x98)
    [ 1.928152] r8:c120bd68 r7:00000000 r6:c100fce8 r5:c120e8d0 r4:c1214658
    [ 1.935136] [<c100fce8>] (__omap_hwmod_setup_all) from [<c0201864>] (do_one_initcall+0xa8/0x204)
    [ 1.944240] r5:c120bd68 r4:00000001
    [ 1.948002] [<c02017bc>] (do_one_initcall) from [<c10010b4>] (kernel_init_freeable+0x1f8/0x2b8)
    [ 1.957016] r10:c107983c r9:c1000700 r8:c1079820 r7:c12a8000 r6:c12a8000 r5:c1088d00
    [ 1.965158] r4:00000001
    [ 1.967854] [<c1000ebc>] (kernel_init_freeable) from [<c0bf31fc>] (kernel_init+0x10/0x148)
    [ 1.976422] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0bf31ec
    [ 1.984560] r4:00000000
    [ 1.987252] [<c0bf31ec>] (kernel_init) from [<c02080a0>] (ret_from_fork+0x14/0x34)
    [ 1.995104] r5:c0bf31ec r4:00000000
    [ 1.998867] Code: e3130080 1a000064 e5943004 e1a00004 (e5942058)
    [ 2.005226] ---[ end trace 8706dc372045be53 ]---
    [ 2.010094] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
    [ 2.010094]
    [ 2.019652] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
    [ 2.019652]

    Any idea please ?

    Regards,

    Chokri

  • Hi Chokri,

    The kernel booting from eMMC has different version.
    [ 0.000000] Linux version 4.4.117 (actia@actia-P5K-Premium) (gcc version 4.9.x 20150123 (prereleas0

    What I am trying to say is, the behavior difference between SD card and eMMC could be because of different kernel images being used. And this issue is not related to booting from eMMC.

    Regards,
    Vishal

  • Please, apply this patch to fix this issue.

    cd <Processor SDK>/board-support/u-boot-<version>/
    git apply 0001-AM57xx-Setup-board-name-to-AM571IDK-if-EEPROM-init-f.patch

    .