Part Number: AM4372
Hi,
In our design, we are connecting a camera sensor and a barcode reader on camera port 0 using a muxer in between to toggle the signals.
The camera is configured to output 8-bit YUV data hence the parallel pins from camera are connected to D[7:0] pins on the camera port. Whereas, the barcode sensor is configured to output 8-bit Y data only. Also the barcode vendor is suggesting to connect the parallel data pins from sensor to D[9:2] pins of the camera port.
Can we connect the 8-bit output from barcode sensor to D[7:0] pins of the camera port? Also, do I need to configure the VPFE for 8-bit raw data?