For example, I am using an OMAP-L138, if I want to disable the SATA and the USB, do I have to build driver in the linux kernel support for SATA and USB in order to put them in a suspend/sleep state?
Would not building in the drivers in the kernel for these devices just disable these devices and enable the lowest power consumption for my OMAP already?