This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: A72_0 target issues

Part Number: TDA4VM

Hi TI,

I have checked the tivxPixelVizNode of the AVP Project. The node includes three targets (DSP1, DSP2, A72_0) as an option in the c66 target.c file , however, on the host file, only two targets were mentioned so I added A72_0 to resolve the target registration issue. But error "target ID is still invalid" is still there.

Do I have to make other changes as well in this node to make it run successfully on A72_0, besides the node working fine on DSPs?

With best regards,

H.M. Owais