HI,
I want use inter Thermal Management functional to get cores temperture, then I checked the psdk_rtos_auto_j7_06_01_00_15 and found the pmlib_thermal.c/.h files.
In the pmlib_thermal.c file we can find PMLIBThermalTurnOnSensor function(line:125), but in the function I can't find these registers in TRM datasheet!! such as (line : 133/137/141/145) and so on,.So where do these configured registers come from??
If we use Thermal Management functional, which registers do we need configure ? Is there a programming sequences?
Please reply as soon as possible!
Regards,
Xie