This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5505: VDDA_PLL drops

Part Number: TMS320C5505

Hi TI Experts,

Customer board using C5505 suffers from garbling UART. (It's based on USBSTK5505)
It occurs in 2 out of 10 units.

Environment
・ UART Baudrate 115200
・ CLKIN 18.432MHz
・ PLL 18.432 / 384 * 2500 = 120MHz

When checking the power supply and clock, the following abnormalities were confirmed.
・ The potential of VDDA_PLL drops during UART communication
・ UART Baudrate drops from 115200 to about 105000Hz

Now ANA_LDOO is connected to VDDA_PLL and VDD_ANA.
We think that power supply is bad, so power supply is changed.

ANA_LDOO---VDDA_PLL---VDD_ANA
↓
1.3V---CVDD ---VDDA_PLL---VDD_ANA

Then the operation improved.

Question 1:
Customer board is not booting with SPI and I2C. Is it okay to input 18.432MHz to CLKIN?

Question 2:
Is there any cause for dropping voltage?

Question 3:
Is it OK to connect the power supply for CVDD (1.3V) to VDDA_PLL and VDD_ANA?

Regards,Rei