I am using a DM6437 on both an Evaluation Board as well as on a custom board.
I am setting up an OV7740 image sensor to work with the DM6437 and am using the VPFE front-end engine. Specifically, I am using the CCDC portion of the the VPFE and trying to use the Preview Engine with the CCDC controller.
I am running into the problem that the Preview Engine is going offline regardless of my setup. I am trying to run it in continuous mode with input directly from the CCDC controller. I am only enabling the CFA function of the preview engine, and providing a CFA table for the preview module.
The CCD controller is working as I am able to put CCD data into the DDR memory.
The goal of this is to get the input from the OV7740 to the CCD controller, and have the data go directly to the Preview Engine.
Do you have any suggestions or advice?