Part Number: TMDSIDK437X
Hi Team,
After a successful build & test of the demo slave application , I am trying to build the full application and encounter compilation issues.
I am following the build instructions in
it seems there is a missing file per the error messages I get (See attached image).
As I am new the ethercat , I have downloaded the stack from ETG. the folder has zip file as well as a slave stack code tool.
1) should I use the zip files as is , or run the tool first and use the tool's output for the demo to work ?
2) How can I tell if the patch was applied successfully ?
3) can you help point me in the right direction with respect to above errors ?
Thanks,
R2