Part Number: TMS320C6678
Hello,
on my design x16 DDR3 is used for ECC.
on the EVB the unused byte is connected as follow:
DQSU 1.5V
DQSUn GND, via 4.7K
DMU GND, via 4.7K
According my understanding the following should be done (refer Micron notes below):
DQSU should be ‘0’
DQSUn should be 1.5V
DMU should be 1.5V
according Micron Notes:
A x16 device's DQ bus is comprised of two bytes. If only one of the bytes needs to be used, use the lower byte for data transfers and terminate the upper byte as noted:
– Connect UDQS to ground via 1kΩ* resistor.
– Connect UDQS# to VDD via 1kΩ* resistor.
– Connect UDM to VDD via 1kΩ* resistor.
– Connect DQ[15:8] individually to either VSS, VDD, or VREF via 1kΩ resistors,* or float DQ[15:8]. *If ODT is used, 1kΩ resistor should be changed to 4x that of the selected ODT
please advise how to connect.
thanks,
Erez