Hello,
I try to add a new codec to my DVSDK 2.0 package running on DM6467, but I cannot find any manual or just advice which familiarizes this issue. I'm a beginner in DaVinci world, so please forgive me if I omitted the "obvious" sources.
I've successfully executed the "encode" demo application which captures the analog input stream to file using H.264 codec. I've read in encode's help and in the source code that the H.264 codec is only supported. I'm pretty sure there is some way to add the new codecs MJPEG, i.e, but I cannot find any advice or hint about that issue. Where can I also find the compatible codecs which can be integrated with my DVSDK?
I will be thankful for your engagement