Part Number: DRA829VXEVM
I've just received my DRA829VXEVM and I'm trying to run the out-of-the box demo.
I assembled the Fusion board and connected IMX390 to it, via FPD-Link and launched the application. However, I can't see the image displayed on the screen.
I've noticed that in the debug messages it is mentioned "IMX390-UB953_D3". Does this mean only D3 module is supported? I have the IMX390 module with same UB953 serializer from Leopard Imaging.
The debug output:
root@j7-evm:/opt/vision_apps# root@j7-evm:/opt/vision_apps# ./run_app_single_cam.sh APP: Init ... !!! APP_LOG: Mapping 0xac000000 ... APP_LOG: Mapped 0xac000000 -> 0xffffa6e90000 of size 262144 bytes MEM: Init ION ... !!! MEM: Initialized ION (fd=4) !!! MEM: Init ION ... Done !!! IPC: Init ... !!! APP_LOG: Mapping 0xac040000 ... APP_LOG: Mapped 0xac040000 -> 0xffffa4ef0000 of size 33161216 bytes APP_LOG: Mapping 0x30e00000 ... APP_LOG: Mapped 0x30e00000 -> 0xffffa7380000 of size 3072 bytes IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! APP: Init ... Done !!! 0.000369 s: VX_ZONE_INIT:Enabled 0.000379 s: VX_ZONE_ERROR:Enabled 0.000383 s: VX_ZONE_WARNING:Enabled 0.000757 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!! 0.000911 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HOST !!! sensor_selection = [0] ldc_enable = [0] num_frames_to_run = [1000000000] is_interactive = [1] 0.005265 s: ISS: Enumerating sensors ... !!! 0.005634 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3 0.005649 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS 0.005654 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI 3 sensor(s) found Supported sensor list: a : IMX390-UB953_D3 b : AR0233-UB953_MARS c : AR0820-UB953_LI Select a sensor [MCU2_1] 197.029064 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CREATE [MCU2_1] 197.029129 s: Sensor at index 0 = IMX390-UB953_D3 [MCU2_1] 197.029160 s: Sensor at index 1 = AR0233-UB953_MARS [MCU2_1] 197.029187 s: Sensor at index 2 = AR0820-UB953_LI a LDC Selection Yes(1)/No(0) LDC Selection Yes(1)/No(0) 1 Sensor selected : IMX390-UB953_D3 Querying IMX390-UB953_D3 4.739035 s: ISS: Querying sensor [IMX390-UB953_D3] ... !!! 4.739241 s: ISS: Querying sensor [IMX390-UB953_D3] ... Done !!! 4.739247 s: ISS: Initializing sensor [IMX390-UB953_D3], doing IM_SENSOR_CMD_PWRON ... !!! [MCU2_1] 201.762791 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_QUERY [MCU2_1] 201.762837 s: Received Query for IMX390-UB953_D3 [MCU2_1] 201.762981 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_PWRON [MCU2_1] 201.763050 s: IM_SENSOR_CMD_PWRON : channel_mask = 0x1 [MCU2_1] 201.763099 s: IMX390_PowerOn : chMask = 0x1 [MCU2_1] 201.763135 s: ub960_cfgScript : ub960I2cAddr = 0x3d [MCU2_1] 201.763159 s: UB960 config start 9.571056 s: ISS: Initializing sensor [IMX390-UB953_D3], doing IM_SENSOR_CMD_CONFIG ... !!! [MCU2_1] 206.594619 s: End of UB960 config [MCU2_1] 206.594826 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CONFIG [MCU2_1] 206.594870 s: Application requested features = 0x358 [MCU2_1] [MCU2_1] 206.594930 s: ub960_cfgScript : ub960I2cAddr = 0x3d [MCU2_1] 206.594957 s: UB960 config start [MCU2_1] 206.834619 s: End of UB960 config [MCU2_1] 206.834655 s: Configuring camera # 0 [MCU2_1] 206.834684 s: ub953 config start : slaveAddr = 0x74 [MCU2_1] 207.201623 s: End of UB953 config [MCU2_1] 207.201701 s: Configuring IMX390 imager 0x40.. Please wait till it finishes 10.809011 s: ISS: Initializing sensor [IMX390-UB953_D3] ... Done !!! Enabling LDC [MCU2_1] 207.832560 s: IMX390 config done [MCU2_1] 207.832601 s: IM_SENSOR_CMD_CONFIG returning status = 0