This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: difference in PC CAffe output and TIDL PC emulation output

Part Number: TDA4VM

Hi,

We have used psdk_rtos_auto_j7_06_02_00_21

tidl j7_01_01_01_01

mmalib_01_01_00_02

We have noticed that the performance between the PC caffe and TIDL PC emulation is very different for the models developed by us.

Our observations are that the model which performs best on PC performs pretty badly in the TIDL PC emulation.

One of the models having precision above 90% is having a lot of false positives when tried on the PC emulation.

I am unable to inser the image files here so will send them via email.

Regards,

Sankalp