Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Hi, TI support team !
I am using TDA4's OSPI interface to connect to a Micron OSPI flash (MT35XL01GBBA) which the working voltage is 3.3V.
The OSPI flash used on TDA4x EVM is MT35XU512ABA which the working voltage is 1.8V.
In uboot, I have cancelled the selection of OSPI flash and hyper flash, and directly use OSPI flash. 0xFF is returned when reading flash ID.
What configuration do I need to modify when I use the OSPI flash (MT35XL01GBBA) which the working voltage is 3.3V?