Part Number: PROCESSOR-SDK-AM335X
Hello,
I am totally new to this. I followed the http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/How_to_Guides/Host/How_to_Setup_Ubuntu_1404_Network_Boot.html to try to boot the beaglebone black over Ethernet. I already made the SYSBOOT 01000b.
However, somehow the beaglebone is stuck before the host can send the SPL file to the BBB. So, the BBB kept requesting and the server kept replying? I'm not sure what cause the issue: DHCP setup, TFTP setup, firewall setup or the BBB itself?
Here is the image from wireshark.
The host IP: 192.168.2.1
The BBB IP seems to be: 192.168.2.5
any input would be appreciated.
Thank you.
Best Regards
Kenny