Part Number: EVMK2GX
Tool/software: Code Composer Studio
The code was built using the procedure in Linux SDK IPC Quick Start Guide which does run using command line on the EVMK2GX.
But when the app_host application is executed using the CCS debugger with the GDB server the fault "Ipc_start: LAD_connect() failed: 4" is reported.
Is there a procedure for debugging the IPC?